This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个关于资料。代码下载的问题



1. www.ti.com.cn/.../spruhj4.pdf中2-13提到

The GIC-400 has a configuration register that allows software to configure each interrupt line to be level-sensitive or edge-sensitive. Because the hardware assumes all shared peripheral interrupts to be pulses, it is the software’s responsibility to ensure that the GICD_ICFGR bits are set up correctly after reset. For more information about the GICD-ICFGR register, see the ARM Generic Interrupt Controller architecture document

请问ARM Generic Interrupt Controller这个文档在哪里可以下载

2. 6630开发板的上的ARM核上有的一些测试应用程序,相应的源代码在哪里可以下载?