您好:
我现在在看6670中有关EDMA3的内容,我想运行C:\Texas Instruments\edma3_lld_02_11_03_03\examples\edma3_driver\src中提供的例子,我自己建立了一个工程,将src中的文件(一些.c和.h文件)拷贝到了我新建的工程里,但是编译的时候会出先无法打开某些头文


不知道为什么找不到这个路径。
我最终的目的是想能运行TI提供的EDMA3的例子,想观察使用EDMA3搬移数据的过程,我该怎么做呢?望指导,谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个头文件是XDC中包含的通用数据类型(如UInt32)定义的头文件,出现这个错误的原因是因为例子工程是基于RTSC建立的,中间使用了XDC Tools,建议你按照在建立工程的时候工程类型选按包含RTSC的工程:

然后在build option中RTSC选项卡中包含一个XDC tools 的版本(你电脑上安装了那个XDC版本就选哪个)