This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

code engine 问题

Other Parts Discussed in Thread: OMAP3530

运行了7次之后,arm+dsp就的程序运行就出现以下错误

root@DevKit8000:/var/volatile/tmp# ./encode                                    

Encode demo started.                                                            

vmap allocation failed: use vmalloc=<size> to increase size.                    

DSP_init status [0x8000800c]                                                  

Unable to handle kernel paging request at virtual address c6714000              

pgd = c24d8000                                                                  

[c6714000] *pgd=8430a011, *pte=00000000, *ppte=00000000                        

Internal error: Oops: 7 [#1]                                                    

Modules linked in: lpm_omap3530 dsplinkk cmemk                                  

CPU: 0    Not tainted  (2.6.28-rc9-omap1 #1)                                    

PC is at OMAP3530_exit+0x5c/0x14c [dsplinkk]                                    

LR is at DSP_exit+0x28/0x30 [dsplinkk]                                          

pc : [<bf00c9b4>]    lr : [<bf00c0fc>]    psr: 80000013                        

sp : c25ddd98  ip : c25dddd8  fp : c25dddd4                                    

r10: bf026864  r9 : bf026860  r8 : c6fa4000                                    

r7 : c6f9b000  r6 : 00008000  r5 : 00000000  r4 : c6714000                      

r3 : 00000000  r2 : c6fa1000  r1 : bf026864  r0 : 00000000                      

Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user              

Control: 10c5387d  Table: 824d8018  DAC: 00000015                              

Process encode (pid: 1650, s