This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【紧急求助】Keystone 1 软件开发包中AIF的问题



TI各位专家: 我在用6700的EVM板开发AIF应用。用了你们提供的Keystone 1 软件开发包其中的AIF2,使用的是LTE 5M 扩展CP,现在测试发现,前3帧数据总是收不到。从打印信息看,Ingress End Of Packet Count 总是比 Egress End Of Packet Count 少360即3帧。应该是从AIF DB到AIF DMA时就已经丢了。请问这个是什么问题,应该怎样解决?我在代码中只使能了aifLinkCfg[1],link rate 4x,numberAxC=1,自环测试。3帧以后的数据收发都是正常的。

前3帧的错误信息:

frame 0: rm_ee_sync_status_change_err

frame 1: rm_ee_sync_status_change_err 和 pe_ee_db_starve_err

frame 2: rm_ee_sync_status_change_err 和 rm_ee_hfnsync_state_err

因为条件限制不能拷贝,只能手工打字了。项目紧急,请各位大侠帮助,谢谢!