This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DDR3降频问题

Expert 1194 points


最近在测试我们自己研发的板子,有四片6678,每片外挂4*512MB=2GB的DDR3,现在遇到如下描述问题:

首先我以数据传输速率为1333Mbps对DDR进行初始化,然后给DDR3中每128KB的内存写入一组递增数,并将DDR中的这组数据与原来模拟的递增数作比较,判断是否有错误,这样共循环16384次就可以把2GB的DDR3测试完毕,在这种情况下,是没有错误发生的。然而在我将数据传输速率降低到800Mbps的时候,就会发生错误。两种速率的参数都是我根据表格和手册计算出来的,我放在附件中。我想问一下,这个问题是是出在软件方面还是硬件方面,希望有人能够指点一下。邮箱地址:gougog3@163.com,如果方便,可以将联系方式发到我邮箱,我们可以详细交流。