This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 Device Cycle Approximate Simulator 使用过程中的问题



您好:

我现在在CCS5.3环境下使用C6670 Device Cycle Approximate Simulator 来评估工程中的算法的实时性,即计算算法总共耗用多少个周期。

选择C6670 Device Cycle Approximate Simulator 之后,算法移植到DSP,我的算法两边没有太复杂的运算,但是for循环嵌套比较多,因为是对图像做处理,循环次数很多都是128*128这种,我使用这个simulator,发现运行起来特别慢,一个函数要运行好几分钟甚至十几分钟,想咨询一下:

1:C6670 Device Cycle Approximate Simulator这个仿真器我直接使用的,需要额外配置什么东西吗?这个仿真器主频是多少?主频可以设吗?因为现在跑的实在太慢了,不利于我调试

2:数据放在L1DRAM、L2SRAM、共享存储区这三个地方,处理速度是不同的吗?是不是放在共享区,数据处理的更慢?

期待您的解答,谢谢啊,初次使用C6670,很多问题不明白。主要是想弄明白用C6670 Device Cycle Approximate Simulator跑我的算法为什么这么慢。