DM8168 + phy芯片8211EG
百兆速度已经通了,但是连接千兆交换机速度还是100M
查看phy 的 CBSR(0XA) 状态只偶尔读到 0x0800 其余时候均为0x0000
对比其他phy寄存器设置,寄存器设置应该是没有问题的。
8211eg 自动协商功能,是由pin_AN[1:0]控制,上电时位拉高状态,
请问,有人知道这个是什么原因吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM8168 + phy芯片8211EG
百兆速度已经通了,但是连接千兆交换机速度还是100M
查看phy 的 CBSR(0XA) 状态只偶尔读到 0x0800 其余时候均为0x0000
对比其他phy寄存器设置,寄存器设置应该是没有问题的。
8211eg 自动协商功能,是由pin_AN[1:0]控制,上电时位拉高状态,
请问,有人知道这个是什么原因吗?
Luo Yu,
你看看下面的e2e讨论是否有帮助?
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/221748
我量了一下phy芯片的自适应 时钟,上电过程中 能在100M和1000M自动切换。但是8168和phy的时钟,只在10M和100M变化。不是道是怎么回事
Luo Yu,
6.2.1 Clock Control
The frequencies for the transmit and receive clocks are fixed by the IEEE 802.3 specification as:
• 2.5 MHz at 10 Mbps
• 25 MHz at 100 Mbps
• 125 MHz at 1000 Mbps