Other Parts Discussed in Thread: TVP5158
我现在用DM6437+TVP5158做四路视频采集。采用的是16位YUV(422)格式,做后端显示的时候,不知道怎么把超级帧格式中的4路信号分开。不知道确定每路信号的第一行。能不能详细讲解,或者把四路视频提取的代码发个我。邮箱:347097655@qq.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Leon Yu 你好:
看你今天还在回复这个帖子,也很愿意分享自己的知识,我现在有些疑问。
首先,你的5158驱动是不是在DM6467上开发的,因为6467前端采集可以达到108MHz,也就说可以做四路D1同时采集,而DM6437采集频率也就是90MHz,楼主说能跑四路720*576我还是比较怀疑的,不知是不是真的可行?
其次,我现在用DM6437+TVP5158做四路视频采集,就像该帖子楼主所说的那种,所有的都跑通了,但是5158到显示屏图像效果明显低于采集卡直接对摄像头采集效果,当然平时看也挺清晰,(摄像头480p)而且行场序不对,已经调过来了,就是说7寸屏看着还挺清晰,到电脑放大后,比采集卡采集的效果要差不少,不知您有没有碰到这个问题
能否提供一下TVP5158 pixel-interleaved 格式的数据分解的参考代码,谢谢了