This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 板SD卡加载UBOOT不成功?

Other Parts Discussed in Thread: AM3352

HI ALL,

1、AM3352 板SD卡加载UBOOT不成功,串口一直打印信息:CCCCCCC.......

2、启动配置为:LCD_DATA[15..0]    0100   0010    0011   0011,启动顺序应该为NAND,  NANDI2C,  MMC0,  UART0

3、目前串口打印C,是否说明系统正在尝试串口启动?那说明MMC0启动失败了?

4、SD卡文件应该不会有问题,尝试别的旧版板子都能够正常加载,换到新的版本就不行?

5、能否通过串口加载uboot,怎么操作,请大家指点下,谢谢

  • 3、目前串口打印C,是否说明系统正在尝试串口启动?那说明MMC0启动失败了?

    Steven:是的,只有MMC0启动失败了,才会进入到UART0,打印CCC

    4、SD卡文件应该不会有问题,尝试别的旧版板子都能够正常加载,换到新的版本就不行?

    Steven:未必是你的文件有问题,也可能是硬件设计上SD卡的借口有问题,需要一步步的确认才知道。

    5、能否通过串口加载uboot,怎么操作,请大家指点下,谢谢

    Steven:参考这个即可:http://processors.wiki.ti.com/index.php/AM335x_U-Boot_User%27s_Guide#Boot_Over_UART

  • Hi Steven,

    1、上电加载uboot的时候不会全部在串口打印C,偶尔会有串口打印C,多数情况下串口没什么反应,SD卡加载不成功就不往下进行了,有遇到过这种情况么?

    2、还有CLKOUT2输出24M的时钟信号,CLKOUT1不输出(外接32K晶体有时候能起震有时候不起震,),如果外部32K晶体不正常应该不会影响系统启动吧?

    3、由于使用TPS65910A3A1 PMU,将VAUX33输出的3.3V接到VDDIO,如下图所示。发现PMU给到AM3352的复位信号PWRONRSTn保持在1.8V,而不是

    3.3V,执行WARM_RESET之后PWRONRSTn会变为3.3V,不正常吧