在DM8148EVM板上,采用EZSDK开发包,能够直接在LCD屏显示图像及支持触摸屏输入,请问采用DVRRDK开发包能够直接在LCD屏显示图像及支持触摸屏输入吗?可以的话,需要对DVRRDK如何进行修改?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在DM8148EVM板上,采用EZSDK开发包,能够直接在LCD屏显示图像及支持触摸屏输入,请问采用DVRRDK开发包能够直接在LCD屏显示图像及支持触摸屏输入吗?可以的话,需要对DVRRDK如何进行修改?谢谢!
Zhang Mingchao,
Linux侧驱动应该是类似,请参考http://processors.wiki.ti.com/index.php/TI81XX_PSP_VPSS_Video_Driver_User_Guide。
在DM8148的EVM板,采用DVRRDK开发包,建立NullSrc-SwMS-DISPLAY,显示的ID选择 SYSTEM_LINK_ID_DISPLAY_1时,编译运行,出现错误为 pObj->displayHndl != NULL的错误信息,当 采用 SYSTEM_LINK_ID_DISPLAY_0和 SYSTEM_LINK_ID_DISPLAY_2时,显示都正常。请问想要LCD屏直接能显示,需要修改那部分的代码,A8内核相关的还是 M3VPSS内核相关的?当M3固件加载成功后,在A8侧的 /sys/devices/platform/vpss/display0~2,以及/sys/devices/platform/vpss/graphics0~2,这可以说明A8驱动正确加载了。