This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关EMIF



TI工程师:
你好 正在看6657的emif 有几个问题咨询下。
1、6657的EMIF16文档中提到
EMIF16 can operate in the following modes:

 WE Strobe Mode

Select Strobe Mode

6748的EMIF16文档中提到
It can be operated in two major modes (see Table 18-14):
 Normal Mode
 Select Strobe Mode

问一下6748的Normal Mode和6657的WE Strobe Mode是不是一回事???

2、6657的文档中提到
WE strobe mode is the default mode supported on CE3.
WE strobe mode is not supported for CE0 - 2.
SS mode is supported for all 4 chip selects.

Async 1 Config Register (A1CR)寄存器的SS位提到
Select Strobe mode.
0x0 – Disable Select Strobe mode
0x1 – Enable Select Strobe mode.

如果A1CR的SS位设为0x0 这时CE0是什么模式 不会是SS mode 如果是WE strobe mode就和“WE strobe mode is not supported for CE0 - 2.” 冲突了啊???

6748中SS位是这样定义的:
0 Normal Mode enabled.
1 Select Strobe Mode enabled.

3、
Connecting to 16-bit ASRAM Connecting to 8-bit ASRAM的示意图中EMIFA23、EMIFA22为啥这么接 有没有更详细的说明???