各位好!
问题RT:
硬件:自己的板卡
软件:基于Helloworld例程修改,替换了GEL等初始化
运行程序后,输出如下:
TCP/IP Stack 'Hello World!' Application
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.2.100
从上面看,好像是已经初始化成功了,可是通过ping 192.168.2.100,会出现超时,或请求失败!请大神帮忙分析原因!谢谢!
PC IP是192.168.2.114