This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5535 程序下载到spi flash无法运行

Other Parts Discussed in Thread: TMS320C5535

IDE版本 CCS6.1.3

芯片:TMS320C5535

问题描述:

1、程序是使用vau模块来检测i2s总线上的音频数据。

2、程序可以正常编译,并使用可以使用debug功能在片上调试运行。

3、将.out文件拷贝到hex55.exe所在目录下;

4、在hex55软件中运行demo.cmd文件,即命令行窗口输入:hex55 demo.cmd(demo.cmd文件内容如下)

-boot
-v5505
-serial8
-b
-o .\mixertest.bin
.\mixer.out

5、使用附件中的工程将bin文件写到flash中。

使用附件的工程可以正常烧写csl库中的gpio demo程序,在flash上运行正常。但是在烧写自己的程序时无法正常运行。

程序的cmd文件内容如下:
-c  /* ROM autoinitialization module */
-a  /* LINK USING C CONVENTIONS      */

-l /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/sdk/lib/sdk_c.a55L
-l /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_c.a55L
-l /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_a.a55L
-l /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/vau/lib/vau_c.a55L

-stack 0x1000
-heap  0x4000
-sysstack 0x1000

MEMORY
{
  DARAM : origin = 0x01000, length = 0x03000
  SARAM1 : origin = 0x4000, length = 0x10000
  SARAM2 : origin = 0x14000, length = 0x10000

  EXTMEM : origin = 0x24000, length = 0x20000

}
                             
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */

SECTIONS
{
  .vau    > EXTMEM
  {
   /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/vau/lib/vau_c.a55L (.text)
  }

  .util    > EXTMEM
  {
    /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_c.a55L (.text)
    /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_a.a55L (.text)
  }

  .text   > EXTMEM
  .cinit  > SARAM2
  .bss    > EXTMEM
  .switch > SARAM1
  .const  > SARAM1
  .sysmem > SARAM1                                             

  .volatileMemBufs    > DARAM
  .nonVolatileMemBufs > SARAM2

  .stack  > SARAM2
  .sysstack > SARAM2
  .data   > SARAM2
  .cio    > SARAM2
  .far    > SARAM2
}

 /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/sdk/lib/sdk_c.a55L
 /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_c.a55L
 /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_a.a55L
 /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/vau/lib/vau_c.a55L


FlashTest.tar.gz
  • 如果能boot demo例程,说明你的boot流程是正确的。

    ROM bootloader会先让所有的接口进入idle状态
    All peripherals are idled (the bootloader un-idles peripherals as it uses them).


    有些port bootloader没用的话不会去使能它,如果你的代码中用到这些port的话,需要先使能。请参考下面wiki网站的例子。
    http://processors.wiki.ti.com/index.php/C5515_Boot-Image_Programmer#Ports_idled_by_bootloader

     

  • 我在ubuntu下使用hex55命令时出现以下提示。

    ./hex55 ./mixer.out -boot -v5505 -serial8 -b -o ./mixer.bin
    Translating to Binary format...
       "./mixer.out"   ==> .vau     (BOOT LOAD)
       "./mixer.out"   ==> .util     (BOOT LOAD)
    error: Starting address of section ./mixer.out(.util) is not aligned to an even
       byte boundary as required for a boot loader of the requested type
       "./mixer.out"   ==> .text     (BOOT LOAD)
       "./mixer.out"   ==> .cinit     (BOOT LOAD)
       "./mixer.out"   ==> .switch     (BOOT LOAD)
       "./mixer.out"   ==> .const     (BOOT LOAD)
       "./mixer.out"   ==> vectors     (BOOT LOAD)

    .map文件中看到util的地址确实是奇数

    .util        0     000311e1  [ 000188f0+] 00000130          *   
                       000311e1  [ 000188f0+] 00000099          *   util_c.a55L : ecoXdaisXlat.o55L (.text)
                       0003127a  [ 0001893d ] 00000055          *   util_a.a55L : utillin2db.o55L (.text)
                       000312cf  [ 00018967+] 00000041          *               : utildb2lin.o55L (.text)
                       00031310  [ 00018988 ] 00000001          *   --HOLE-- [fill = 20]


    然后我将cmd文件中util注释掉就可以正常生成bin文件了

    /*

    .util    > EXTMEM
      {
        /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_c.a55L (.text)
        /home/ly/ti/volib_C55_CPU3_2_1_0_1/packages/ti/mas/util/lib/util_a.a55L (.text)
      }

    */

    请问这是为什么呢?为什么util加载的地址会是奇数?其他的地址都是偶数起始啊。

    附件是.map文件

    mixer.map.tar.gz