This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm3730 android2.3 源码不全,文件系统编译出错



大家好,知道的,知道的帮助一下我这个初学者,我下载了dm3730 android的源码包TI_Android_GingerBread_2_3_Sources.tar.gz,按文档TI-Android-GingerBread-2.3-DevKit-1.0_DeveloperGuide.pdf

#./.repo/repo/repo sync --local-only

Syncing work tree: 100% (169/169), done.  

我编译文件系统时出现如下:

#make TARGET_PRODUCT=omap3evm OMAPES=5.x -j8

============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=2.3
TARGET_PRODUCT=omap3evm
TARGET_BUILD_VARIANT=eng
TARGET_SIMULATOR=
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=GRH55
============================================
find: `core/java': No such file or directory
find: `graphics/java': No such file or directory
find: `location/java': No such file or directory
find: `media/java': No such file or directory
find: `opengl/java': No such file or directory
find: `sax/java': No such file or directory
find: `telephony/java': No such file or directory
find: `wifi/java': No such file or directory
find: `vpn/java': No such file or directory
find: `keystore/java': No such file or directory
find: `voip/java': No such file or directory
find: `core/config/ndebug': No such file or directory
find: `test-runner/src': No such file or directory
find: `core/config/sdk': No such file or directory
find: `core/java': No such file or directory
find: `graphics/java': No such file or directory
find: `location/java': No such file or directory
find: `media/java': No such file or directory
find: `opengl/java': No such file or directory
find: `sax/java': No such file or directory
find: `telephony/java': No such file or directory
find: `wifi/java': No such file or directory
find: `vpn/java': No such file or directory
find: `keystore/java': No such file or directory
find: `voip/java': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
make: *** No rule to make target `out/host/linux-x86/bin/aapt', needed by `out/target/common/obj/JAVA_LIBRARIES/core_intermediates/javalib.jar'. Stop.
make: *** Waiting for unfinished jobs....
host SharedLib: libneo_util (out/host/linux-x86/obj/lib/libneo_util.so)
host StaticLib: libhost (out/host/linux-x86/obj/STATIC_LIBRARIES/libhost_intermediates/libhost.a)
echo out/host/linux-x86/obj/STATIC_LIBRARIES/libhost_intermediates/pseudolocalize.o out/host/linux-x86/obj/STATIC_LIBRARIES/libhost_intermediates/CopyFile.o | xargs ar crsP out/host/linux-x86/obj/STATIC_LIBRARIES/libhost_intermediates/libhost.a

很多文件找不到,因为找不到编译终止,不是都完全同步了吗Syncing work tree: 100% (169/169), done.  请问接下来应该怎么办呢