This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168启动问题,请帮忙看下



8168启动时,有时卡在这里,请问是何原因?

Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev sda.
EXT3-fs (sda): error: can't find ext3 filesystem on dev sda.
EXT2-fs (sda): error: can't find an ext2 filesystem on dev sda.
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev sda.
ISOFS: Unable to identify CD-ROM format.
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (sda1): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (sda1): using internal journal
EXT3-fs (sda1): recovery complete
EXT3-fs (sda1): mounted filesystem with writeback data mode
ALSA: Restoring mixer settings...
Configuring network interfaces... ifup: ignoring unknown interface eth0
ifup: ignoring unknown interface eth1
done.
Setting up IP spoofing protection: rp_filter.
Thu Jun 25 03:08:00 UTC 2015
SysLink version : 2.20.02.20
SysLink module created on Date:Sep 29 2014 Time:18:19:50
Trace enabled
Trace SetFailureReason enabled
DMA: Module install successful, device major num = 249
DRV: Module install successful
DRV: Module built on Sep 29 2014 18:20:16
VPSS_FVID2: create handle is NULL
VPSS_SYSTEM: failed to create handle
VPSS_CORE : failed to init system
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
ti81xxfb: Unknown symbol vps_grpx_get_ctrl (err 0)
ti81xxfb: Unknown symbol vps_grpx_get_num_grpx (err 0)
ti81xxhdmi: Unknown symbol TI81xx_un_register_display_panel (err 0)
ti81xxhdmi: Unknown symbol TI81xx_register_display_panel (err 0)