This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678多核DSP CCS编译警告,求助啊~~谢谢(用的是论坛置顶提供的例程)CCS5.1 编译器7.4



Description Resource Path Location Type
#10247-D creating output section "vecs" without a SECTIONS GPIO C/C++ Problem
Build variable 'PDK_INSTALL_PATH' cannot be resolved. GPIO properties TI Problem Marker
Build variable 'PDK_INSTALL_PATH' cannot be resolved. GPIO properties TI Problem Marker
Invalid project path: Include path not found (\packages). GPIO pathentry Path Entry Problem
Invalid project path: Include path not found (\packages\ti\csl). GPIO pathentry Path Entry Problem
Invalid project path: Include path not found (D:\ti\project\test3\common). GPIO pathentry Path Entry Problem
This project was created using a version of compiler that is not currently installed: 7.4.4 [C6000]. Another version of the compiler will be used during build: 7.4.1. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. GPIO properties TI Problem Marker