关于OMAPL138的双核应用我有一个疑惑,我想在DSP端应用MASP+I2C+EDMA外设做音频采集,困惑如下:
1、芯片角度下,如果在DSP和ARM同时打开某一外设中断,事件到来时DSP和ARM是否会同时产生中断?
2、在ARM上运行TI提供的linux-3.3系统,系统驱动中已经注册了相应的中断,如果我在DSP再操作该外设,是否影响linux的运行?
3、希望较高实时性实现音频数据采集+处理+发送,处理算法在DSP端实现,每帧数据较短,96ksps下20~50点每帧,什么方法较好,有人建议完全在linux上控制外设避免冲突,采样数据传入DSP,计算结果传出DSP,在经过linux发送,但是这样担心linux实时性发生问题,所以倾向于DSP端直接访问外设,向各位TI专家求建议。