This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OMAPL138 USB的DMA问题



各位专家好,

请教一个问题,我们在使用OMAPL138开发产品,使用的软件平台是TI的StarterWare_1_10_04_01。

测试的工程是:\build\armv5\cgt_ccs\omapl138\evmOMAPL138\usb_dev_msc 中的usb, 工程是在omap138 arm 端运行的。

问题是:

当打开 DMA_MODE 选项时时  向udisk拷入大的文件(大约1.5M) 时每次写入64K时usb 通信就会中断。关掉 DMA_MODE 时 操作正常,但是写入速度会很慢,大约要3秒 。请问题在DMA  的使用有那些注意事项,谢谢。

Kent Lu