This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 ISIF



你好,目前我没有使用sensor,图像是由一个摄像机输入的,摄像机又通过FPGA,FPGA和dm385是通过ISIF连接,由于我使用的开发包是IPNCV3.8,这个开发包默认是针对MN34041,所以FPGA发送的数据分辨率也是1920*1080的RAW数据,FPGA采用外同步方式,每秒25帧数据,但是DM385这边只能收到几帧,打印如下:

queue id:65538
Creat queue id:98307
queue id:98307
IPNC_3.80.00 (root@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
[m3video] Remote Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040

[host] Attached to slave procId 1.

[host] Attached to slave procId 0.

[host] Loaded file ./firmware/ipnc_rdk_fw_m3vpss.xem3 on slave procId 1.

[host] Started slave procId 1.

[host] Loaded file ./firmware/ipnc_rdk_fw_m3video.xem3 on slave procId 0.

[host] Started slave procId 0.

[host] After Ipc_loadcallback status [0x00000000]

[host] After Ipc_loadcallback status [0x00000000]
[m3video] ***** SYSTEM : Frequency <ORG> - 200000000, <NEW> - 200000000

[host] After Ipc_startcallback status [0x00000000]

[host] After Ipc_startcallback status [0x00000000]
[m3vpss ] ***** SYSTEM : Frequency <ORG> - 200000000, <NEW> - 200000000
[m3video]
[m3vpss ] notify_attach rtnVal 0
[m3video] *** UTILS: CPU KHz = 400000 Khz ***
[m3vpss ] initProxyServer rtnVal 0
[m3video]
[m3vpss ]
[m3video] 39: SYSTEM : System Common Init in progress !!!
[m3vpss ] *** UTILS: CPU KHz = 400000 Khz ***
[m3video] 40: SYSTEM: IPC init in progress !!!
[m3vpss ]
[m3video] 40: SYSTEM: Attaching to [HOST] ...
[m3vpss ] 71: SYSTEM : System Common Init in progress !!!
[m3video] 89: SYSTEM: Attaching to [HOST] ...
[m3vpss ] 71: SYSTEM: IPC init in progress !!!
[m3video] 92: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
[m3vpss ] 71: SYSTEM: Attaching to [HOST] ...
[m3video] 92: SYSTEM: Attaching to [VPSS-M3] ...
[m3vpss ] 121: SYSTEM: Attaching to [HOST] ...
[m3video] 142: SYSTEM: Attaching to [VPSS-M3] ...
[m3vpss ] 124: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
[m3vpss ] 124: SYSTEM: Attaching to [VIDEO-M3] ...
[m3video] 174: SYSTEM: Attaching to [VPSS-M3] ... SUCCESS !!!
[m3vpss ] 173: SYSTEM: Attaching to [VIDEO-M3] ...
[m3video] 174: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
[m3vpss ] 174: SYSTEM: Attaching to [VIDEO-M3] ... SUCCESS !!!
[m3vpss ] 174: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
[m3vpss ] 174: SYSTEM: Creating MsgQ [VPSS-M3_MSGQ] ...
[m3vpss ] 175: SYSTEM: Creating MsgQ [VPSS-M3_ACK_MSGQ] ...
[m3vpss ] 177: SYSTEM: Notify register to [HOST] line 0, event 12 ...
[m3vpss ] 177: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ...
[m3vpss ] 177: SYSTEM: IPC init DONE !!!
[m3vpss ] 188: MEM: Shared Region 2: Base = 0xb8000000, Length = 0x06900000 (
[m3vpss ] 188: MEM: Shared Region 1: Base = 0x89000000, Length = 0x03b00000 (
[m3vpss ] Received character 's'
[m3vpss ] 191: SYSTEM : System Common Init Done !!!
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
[m3video] Remote Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
[m3video] 274: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
[m3video] 275: SYSTEM: Creating MsgQ [VIDEO-M3_MSGQ] ...
[m3video] 275: SYSTEM: Creating MsgQ [VIDEO-M3_ACK_MSGQ] ...
[m3video] 277: SYSTEM: Notify register to [HOST] line 0, event 12 ...
[m3video] 277: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ...
[m3video] 278: SYSTEM: IPC init DONE !!!
[m3video] 288: MEM: Shared Region 2: Base = 0xb8000000, Length = 0x06900000 (
[m3video] 289: MEM: Shared Region 1: Base = 0x89000000, Length = 0x03b00000 (
[m3video] 291: SYSTEM : System Common Init Done !!!
[m3video] Received character 's'
queue id:65538
Creat queue id:131076
queue id:131076

CPU is TI812x

*****************************************************************

IPNC BUILD VERSION: IPNC RDK VERSION 03.80.00.05 (LOW POWER)

*****************************************************************

DEMOCFG Value : 0
Videocodecmode : 8
Videocodecres : 0
streamtype : 2

vsenable : 0
./bin/ipnc_rdk_mcfw.out TRISTREAM TRIPLE_H264 TI2A AEWB 1080P_D1 H264 HIGH_SP&
Creat queue id:163845
queue id:163845
queue id:65538
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
[m3video] Remote Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
ApproDrvInit: 7
queue id:163845
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
[m3video] Remote Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
[m3video] Remote Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
[m3video] 490: SYSTEM : System Video Init in progress !!!
[m3vpss ] 490: SYSTEM : System VPSS Init in progress !!!
[m3video] 491: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
[m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to ISS_PLATFORM_CPU_REV_1
[m3video] 492: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
[m3vpss ] 491: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
[m3video] 492: SYSTEM: ListElem Shared Addr = 0xbe984700
[m3vpss ] 492: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
[m3video] 494: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
[m3vpss ] 492: SYSTEM: ListElem Shared Addr = 0xbe987680
[m3video] 495: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
[m3vpss ] 494: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
[m3video] 495: SYSTEM: ListElem Shared Addr = 0xbe98b100
[m3vpss ] 495: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
[m3vpss ] 495: SYSTEM: ListElem Shared Addr = 0xbe98e080
[m3video] 505: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_29] in region 0 ...
[m3video] 506: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_29] in region 0 ...
[m3video] 506: SYSTEM: ListElem Shared Addr = 0xbe991580
[m3video] 508: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_30] in region 0 ...
[m3vpss ] 509: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_24] in region 0 ...
[m3video] 509: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_30] in region 0 ...
[m3vpss ] 509: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_24] in region 0 ...
[m3video] 509: SYSTEM: ListElem Shared Addr = 0xbe9ab200
[m3vpss ] 510: SYSTEM: ListElem Shared Addr = 0xbe9c4e80
[m3video] 511: HDVICP: Doing PRCM for IVAHD[0] ...
[m3vpss ] 512: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_25] in region 0 ...
[m3video] 511: HDVICP: PRCM for IVAHD[0] ... DONE.
[m3vpss ] 513: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_25] in region 0 ...
[m3video] 512: SYSTEM : Initializing Links !!!
[m3vpss ] 513: SYSTEM: ListElem Shared Addr = 0xbe9e4880
[m3vpss ] 516: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_26] in region 0 ...
[m3video] 512: SYSTEM : FREE SPACE : System Heap = 2088976 B, Mbx = 102
[m3vpss ] 517: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_26] in region 0 ...
[m3vpss ] 517: SYSTEM: ListElem Shared Addr = 0xbea04280
[m3video] 513: SYSTEM : FREE SPACE : SR0 Heap = 15842048 B (15 MB)
[m3video] 513: SYSTEM : FREE SPACE : Frame Buffer = 110100352 B (104 MB)
[m3vpss ] 524: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_29] in region 0 ...
[m3vpssDMA: Module install successful, device major num = 247
] 524: SYSTEM:DRV: Module install successful
Creating ListMPDRV: Module built on Sep 24 2016 02:51:40
[VPSS-M3_IPC_IN_29] in region 0 ...
[m3video] 513: SYSTEM : FREE SPACE : Bitstream Buffer = 61865856 B (58 MB)
[m3vpss ] 524: SYSTEM: ListElem Shared Addr = 0xbea23c80
[m3vpss ] 527: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_30] in region 0 ...
[m3video] 514: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
[m3vpss ] 527: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_30] in region 0 ...
[m3video] 515: SYSTEM : FREE SPACE : Tiler Buffer = 128 B (0 MB) - TILE
[m3vpss ] 528: SYSTEM: ListElem Shared Addr = 0xbea3d900
[m3video] Entered the MctnfLink_init()
[m3vpss ] 530: SYSTEM : Device Init in progress !!!
[m3vpss ] Iss_init called !!!!!!
[m3vpss ] CPIS_init DONE !!!!!!
[m3vpss ] 536: SYSTEM : Device Init in progress DONE !!!
[m3video] 575: SYSTEM : Initializing Links ... DONE !!!
[m3video] 575: SYSTEM : System Video Init Done !!!
[m3vpss ] 583: SYSTEM : System VPSS Init Done !!!
[m3vpss ] 584: UTILS: DMA: HWI Create for INT62 !!!
[m3vpss ] 584: SYSTEM : Initializing Links !!!
[m3vpss ] 584: SYSTEM : FREE SPACE : System Heap = 1684624 B, Mbx = 102
[m3vpss ] 584: SYSTEM : FREE SPACE : SR0 Heap = 15372416 B (14 MB)
[m3vpss ] 585: SYSTEM : FREE SPACE : Frame Buffer = 105790336 B (100 MB)
[m3vpss ] 585: SYSTEM : FREE SPACE : Bitstream Buffer = 61865856 B (58 MB)
[m3vpss ] 585: SYSTEM : FREE SPACE : Tiler Buffer = 128 B (0 MB) - TILE
[m3vpss ] 667: SYSTEM : Initializing Links ... DONE !!!
[m3vpss ] Received character 't'
[c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
DMA: ChannelID allocated:4
[m3video] RemotDMA: ChannelID allocated:5
e Debug Shared Memory @ 0xbff05020
[m3vpss ] Remote Debug Shared Memory @ 0xbff0a040
[m3video] Received character 't'
/dev/mem opened.
Phy Addr : 0x48180e00 Data : 0x00030000
Phy Addr : 0x48180e10 Data : 0x00000007
Phy Addr : 0x48180e04 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000000
Phy Addr : 0x48180800 Data : 0x00000001
Phy Addr : 0x48180820 Data : 0x00070000
Phy Addr : 0x48180824 Data : 0x00030002
Phy Addr : 0x48180e04 Data : 0x00000000
Phy Addr : 0x48180e00 Data : 0x00030000
Phy Addr : 0x48180e10 Data : 0x00000007
Phy Addr : 0x48180e04 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000000
Phy Addr : 0x48180800 Data : 0x00000001
Phy Addr : 0x48180820 Data : 0x00070000
Phy Addr : 0x48180824 Data : 0x00030002

[host] Application Start Completed

[host] 0: SYSTEM: System Common Init in progress !!!

[host] 1: SYSTEM: IPC init in progress !!!

[host] 21: SYSTEM: CPU [DSP] is NOT available on this platform !!!

[host] 21: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [0] !!!

[host] 21: SYSTEM: CPU [VPSS-M3] syslink proc ID is [1] !!!

[host] 21: SYSTEM: CPU [HOST] syslink proc ID is [2] !!!

[host] 22: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...

[host] 25: SYSTEM: Creating MsgQ [HOST_MSGQ] ...

[host] 27: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...

[host] 28: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...

[host] 29: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...

[host] 31: SYSTEM: Notify register to [VIDEO-M3] line 0, event 12 ...

[host] 32: SYSTEM: Notify register to [VPSS-M3] line 0, event 12 ...

[host] 33: SYSTEM: IPC init DONE !!!

[host] 37: SYSTEM: Creating ListMP [HOST_IPC_OUT_29] in region 0 ...

[host] 39: SYSTEM: Creating ListMP [HOST_IPC_IN_29] in region 0 ...

[host] 41: SYSTEM: ListElem Shared Addr = 0x40da8580

[host] 42: SYSTEM: Creating ListMP [HOST_IPC_OUT_30] in region 0 ...

[host] 44: SYSTEM: Creating ListMP [HOST_IPC_IN_30] in region 0 ...

[host] 46: SYSTEM: ListElem Shared Addr = 0x40dc2200

[host] 49: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...

[host] 51: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...

[host] 52: SYSTEM: ListElem Shared Addr = 0x40ddbe80

[host] 54: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...

[host] 56: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...

[host] 57: SYSTEM: ListElem Shared Addr = 0x40dfb880

[host] 59: SYSTEM: Creating ListMP [HOST_IPC_OUT_26] in region 0 ...

[host] 61: SYSTEM: Creating ListMP [HOST_IPC_IN_26] in region 0 ...

[host] 63: SYSTEM: ListElem Shared Addr = 0x40e1b280

[host] 63: SYSTEM: System Common Init Done !!!

[host] Vsys_allocBuf - addr = 0x4c7d4000,size = 65011712
##########pInfo->totalsize 63897600

[host] MemMng_memcpy_open:OSA_dmaOpen passed with ch id = 4

[host] CacheMng_MemCpy_open:OSA_dmaOpen passed with ch id = 5

[host] MCFW_IPCFRAMES:App_ipcFramesSendRecvFxn:Entered...
[host] Vsys_allocBuf - addr = 0x51814000,size = 27661

[host] DCC buffer allocated for size 27661

[host] DCC Default File Intialization Done

[host]
********** LOW POWER USECASE ********

[host] ********* Entered Tri Streaming usecase - H264 1080p @60fps + H264 D1 @*


[host] 89: MCFW : CPU Revision [ES1.0] !!!

[host] 89: MCFW : Detected [UNKNOWN] Board !!!

[host] 89: MCFW : Base Board Revision [UNKNOWN] !!!
[m3vpss ] 845: CAMERA: Create in progress !!!
[m3vpss ] Channel Num Stream 0 Ch 0 ChannelNum 0
[m3vpss ] Channel Num Stream 1 Ch 0 ChannelNum 1
[m3vpss ] 845: CAMERA: VIP0 PortA camera mode is [ 8-bit, Non-mux Embedded Sy
[m3vpss ] I2C: timed out in wait_for_bb: I2C_IRQSTATUS=1000 !!!
[m3vpss ] 5846: CAMERA: VIP 0: VID DEC 268436738 (0x10): 0002:20202020:2020208
[m3vpss ] Iss_captCreate:1661
INIT: Entering runlevel: 5
[m3vpss ] 6058: CAMERA: Create Done !!!
inside autorun
sbulla: unknown partition table
Starting telnet daemon [m3vpss ] 6149: CAMERA: Detect video in progress !!!
[m3vpss ] 6149: CAMERA: Detect video Done !!!
[m3vpss ] 6225: DUP : Create Done !!!
[m3vpss ] DCC server task running
[m3vpss ] 6235DMA: ChannelID allocated:6
: MERGE : CreaDMA: ChannelID allocated:7
te Done !!!
[m3vpss ] {SWOSD} edma3Handle->tccVal = 36
[m3vpss ] {SWOSD} edma3Handle->chId = 36
[m3vpss ] {SWOSD} edma3Handle->tccVal = 37
[m3vpss ] {SWOSD} edma3Handle->chId = 37
[m3vpss ] {SWOSD} edma3Handle->tccVal = 38
[m3vpss ] {SWOSD} edma3Handle->chId = 38
[m3vpss ] 6245: SYSTEM: Opening MsgQ [HOST_MSGQ] ...

[host] Vsys_eventHandler:OSA_dmaOpen passed with ch id = 6

[host] Vsys_eventHandler:OSA_dmaOpen passed with ch id = 7
[m3vpss ] 6244: SWOSD : Create Done !!!
[m3vpss ] 6317: IPC_OUT_M3 : Create in progress !!!
[m3vpss ] 6318: IPC_OUT_M3 : Create Done !!!
[m3video] 6355 sbulla: unknown partition table
: IPC_IN_M3 : Create in progress !!!
[m3video] 6356: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3video] 6356: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3video] 6359: IPC_IN_M3 : Create Done !!!
[m3video] 6367: ENCODE: Create in progress ... !!!
.
Starting syslogd/klogd: done


_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org DM385_IPNC ttyO0
[m3video] 6499: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1984, 1984) [PR

Arago 2011.09 DM385_IPNC ttyO0

DM385_IPNC login: root (automatic login)
[m3video] ENCLINK_H264:HEAPID:0 USED:13272
[m3video] 6584: ENCODE: Creating CH1 of 720 x 480, pitch = (720, 720) [PROGRE
root@DM385_IPNC:~#
[host] IpcBitsInLink_tskMain:Entered
[host] 5854: IPC_BITS_IN : Create in progress !!!

[host] 5854: IPC_BITS_IN : ListMPOpen start !!!

[host] 5854: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_29] ...

[host] 5856: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_29] ...

[host] 5858: IPC_BITS_IN : ListMPOpen done !!!

[host] 5859: IPC_BITS_IN : System_linkGetInfo done !!!

[host] 5860: IPC_BITS_IN : Create Done !!!

[host] USECASE SETUP DONE
[m3vpss ] 6616: CAMERA: Start in progress !!!
[m3video] ENCLINK_H264:HEAPID:0 USED:11720
[m3vpss ] 6616: CAMERA: Start Done !!!
[m3video] 6668: ENCODE: Creating CH2 of 1920 x 1080, pitch = (1984, 1984) [PR
[m3video] ENCLINK_JPEG:HEAPID:0 USED:4368
[m3video] 6670: ENCODE: All CH Create ... DONE !!!
[m3video] ENCLINK:HEAPID:0 USED:29688
[m3video] 6672: ENCODE: Create ... DONE !!!
[m3video] 6635: VSTAB : Alg Create Done !!!
[m3video] 6635: VSTAB : Create Done !!!
[m3video] 6674: IPC_BITS_OUT : Create in progress !!!
[m3video] 6676: IPC_BITS_OUT : Create Done !!!

[host]
Application Run Completed

[host] ITT server task running !!!

[host]
ITT ittServer_run

[host] ITT Server Message initialization successful

[host]
ITT capture task created

[host] DCC server Message ques is open succefully

[host] Setting cmd <1> in message <40c54c00>

[host] Posting message <40c54c00> in QId <10002>
[m3vpss ] Command 1 recived from HOST A8

[host] Response from M3 is : 1

[host] Response from M3 is : 1

[host] Default parameters were sent sucessfully

[host] Server Socket created with ID <22>
[m3vpss ] Command 2 recived from HOST A8
[m3vpss ] New DCC data of size <27661>
[m3vpss ] Call to VNF_LINK_CMD_UPDATE_DCC -1
mkdosfs 3.0.12 (29 Oct 2011)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
There is 1 reserved sector.
Root directory contains 512 slots and uses 32 sectors.
Volume ID is cefdbba0, no volume label.
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
g_file_storage gadget-lun0: ro=0, nofua=0, file: /dev/sbulla
Simple mixer control 'PGA',0
Capabilities: cvolume cswitch penum
Capture channels: Front Left - Front Right
Limits: Capture 0 - 119
Front Left: Capture 80 [67%] [40.00dB] [on]
Front Right: Capture 80 [67%] [40.00dB] [on]
queue id:0
./boa: /usr/lib/libssl.so.1.0.0: no version information available (required by )
./boa: /usr/lib/libcrypto.so.1.0.0: no version information available (required )
ApproDrvInit: 3
queue id:163845
queue id:0
queue id:32769
queue id:0
TimeOut occure in boot_proc.
Program exit.
TimeOut occure in boot_proc.
Program exit.

[host]
Usecase is Active !!!

[host]
Usecase is Active !!!
[m3vpss ] CT: 1000, 3dlut index:0
[m3vpss ] 70664: CAMERA: Dequeued 1 frames !!!
[m3vpss ] 70664: CAMERA: Dequeued 1 frames !!!
[m3video] Channel:0 inputframerate:60 targetfps:60
[m3video] Channel:1 inputframerate:30 targetfps:60
[m3video] Channel:2 inputframerate:60 targetfps:5
[m3vpss ] 70689: CAMERA: Queued back 1 frames !!!
[m3vpss ] 70701: CAMERA: Queued back 1 frames !!!

[host]
Usecase is Active !!!
net_get_netmask: ioctl SIOCGIFNETMASK: Cannot assign requested address
killall: dhcpcd: no process killed
PHY 0:00 not found
PHY 0:01 not found
[m3vpss ] 135286: CAMERA: Dequeued 1 frames !!!
[m3vpss ] 147819: CAMERA: Dequeued 1 frames !!!
[m3vpss ] 147819: CAMERA: Dequeued 1 frames !!!
[m3vpss ] 147819: CAMERA: Fields = 8 (fps = 0), Total Resets = 0 (Avg 0 ms pe)

[host]
Usecase is Active !!!

  • Xin Jin,

    先确认一下M3 bios下配置的频率和你实际配置的M3的频率是否一致。

    System_common.h

    /* Frequency values of various cores set explicitly during system init */

    #define SYSTEM_M3CORE_FREQ         (200*1000*1000)               

    确认一下是否VDINT中断是否有收到每秒25个?

      

  •  你好:我确认了一下SYSTEM_M3CORE_FREQ         (200*1000*1000)  是对的。

    我有点疑问,我这几天看程序,虽然我这个开发包是针对MN34041的,但我没有看到那里有针对MN34041进行具体的寄存器设置;比如:ipipe_reg->SRC_VSZ,ipipe_reg->SRC_HSZ等。

    所以我今天添加了

         ipipe_reg->SRC_VSZ  = 1079;
        ipipe_reg->SRC_HSZ  = 1919;
        isif_reg->LNH = 1079;
        isif_reg->LNV = 1919;
        rsz_reg->SRC_VSZ    = 1079;
        rsz_reg->SRC_HSZ    = 1919; 
    目前和以前好了很多,目前不断能收到数据,但是帧率不对,大约5秒中左右收到几帧,VDINT中断也是5秒中收到几个中断。
  • jin xin 说:
    我确认了一下SYSTEM_M3CORE_FREQ         (200*1000*1000)  是对的。

    请问你uboot里面配置的M3是200Mhz么?

  • U-Boot 2010.06 (Sep 26 2016 - 19:22:21) DM385_IPNC_3.80.00

    DM385-GP rev 1.1

    ARM clk: 600MHz
    DDR clk: 400MHz
    L3 clk: 200MHz
    IVA clk: 220MHz
    ISS clk: 400MHz
    DSP Default OFF
    DSS Default OFF

  • jin xin 说:
    我有点疑问,我这几天看程序,虽然我这个开发包是针对MN34041的,但我没有看到那里有针对MN34041进行具体的寄存器设置;比如:ipipe_reg->SRC_VSZ,ipipe_reg->SRC_HSZ等。

    ISP的配置有些是通用的,如果MN34041有特殊的,有专门的配置,你可以在代码里面搜索MN34041。你现在的FPGA时序是完全按照MN34041的输出配置的么?包括行同步/帧同步的极性等。我建议你看看下面的文章,把现有的ISP采集配置和你FPGA输出的时序好好对一下:

    《DM368 视频前端信号采集详解》- 该文对理解DM8127/DM38x的并口采集也有帮助
    http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/70099.aspx

  • 那个pdf我看了很多边,我之所以改

         ipipe_reg->SRC_VSZ  = 1079;
        ipipe_reg->SRC_HSZ  = 1919;
        isif_reg->LNH = 1079;
        isif_reg->LNV = 1919;
        rsz_reg->SRC_VSZ    = 1079;
        rsz_reg->SRC_HSZ    = 1919;就是按照那个PDF设置的,FPGA目前按照我现在设置的发送数据(发送1920*1080字节的RAW数据,时钟74.25MHZ,8位宽度),VD和HD都是高电平有效。
    还有就是FPGA发送的数据是模拟数据,就是一个累加数。
     
  • Xin Jin,

    FPGA发送的数据内容不重要,重要的还是同步信号和pclk。

    VDINT应该是和外部VD信号是完全一致的。VDINT0现在配置的值是多少?

  • VDINT0这个我没有改,是默认的。

  • 我怎么确定这个VDINT0,是外部VD的需要的pclk上升沿的个数吗。

  • Xin Jin,

    请参考下面的帖子:

    https://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/p/106886/287716.aspx