This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大侠:
刚做的C6657电路板回来测试,发现CVDD对地阻抗7欧姆,VCC1V0对地阻抗26欧姆,请问正常吗?可以上电不?不胜感激
你拿个没焊的芯片测一下对比。
找了一个没焊的芯片,cvdd与vcc1v对地都是27欧左右,是否可确认焊接的芯片问题呢?
27ohm跟你在板子上测的26ohm不是差不多么,为什么还认为焊接有问题呢?
但是cvdd 本来是27焊接后 变成7了