This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无法连接到66AK2H14的ARM核

Other Parts Discussed in Thread: 66AK2H14

大家好,

软件版本为:CCS v6.1.3,Processork SDK pdk_k2hk_4_0_2/pdk_keystone2_3_01_04_07/processor_sdk_rtos_k2hk_3_00_00_04.

在自己做的板子上做的测试,板子上有两片66AK2H14,设计为菊花链方式,一个JTAG调试口。

仿真器为Wintech XDS560v2的老版(需要外部的DC电源供电,新版直接USB供电,咨询过Wintech的工程师,说可以支持66AK2H14的调试)

66AK2H14被设置为Sleep mode,BootMode pin(GPIO0~15)由FPGA控制,设置为0x0000_0000_0000_0000.

板子上电后,JTAG测试通过。通过CCS可以连接到两片66AK2H14的任意一个DSP核,并可以跑程序没有问题。

但是这个时候连接66AK2H14的ARM核,则出现连不上的问题,如下图。

请教一下怎么分析解决?

1. 仿真器不支持?

2. 我已经检查了ARM的电源(ARM core fixed supply CVDDT1 0.95V)、时钟(ARMCLKP/N 125MHz)都没有问题。而且JTAG可连接DSP核,那么JTAG链路应该也没问题。感觉硬件就没问题了吧?

3. 按照66AK2H14的手册中下图

ARM核用的是SYSCLK1?SYSCLK1是由SYSCLK分出来的,那么ARMCLKP/N是用来做什么的?

谢谢!