This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6748的Programmable Real-Time Unit Subsystem (PRUSS)

Other Parts Discussed in Thread: AM1808, PRU-SWPKG

因为项目需要,需使用PRU,目前有如下几个疑问:

1、看到的PRU资料都是与达芬奇系列相关的。资料是否是通用的?

      如:training.ti.com/sitara-processors-building-blocks-for-pru-development-summary

2、看到PRU可用C开发,C6748的PRU上是不是能用C?

3、在CCS(6.0.1)中C6748没有创建PRU工程的选项。A335X等就有。

       是不是C6748的PRU不能在CCS下开发?

谢谢!

  • 1,6748上面的PRU是第一代的,和达芬奇的有点细微差别,基本是一样的。

    可以看看

    http://www.ti.com/tool/pru-swpkg?keyMatch=am1808%20pru&tisearch=Search-EN-Everything

    http://processors.wiki.ti.com/index.php/Soft-UART_Implementation_on_OMAPL_PRU_-_Software_Users_Guide?keyMatch=am1808%20pru&tisearch=Search-EN-Everything

    3,可以试试OMAPL138或者AM1808看看能否创建CCS工程。

  • 你提供的链接早些时候也看过。 wiki上明确说了 The PRU Software Support Package provides support for the PRU-ICSS Subsystem in AM335x, AM437x, and AM57xx devices. This package contains 并没有说c6748.所以怀疑工具等是否也针对c6748。 omapl138创建倒没试过,没带电脑,明天试下。
  • 选择L138就出来了。C6748的配置没把PRU加进去。说明这个C compiler是支持C6748上的PRU的。

  • 1、PRU包含了PRUSS(Programmable Real-Time Unit Subsystem)和PRU-ICSS(Programmable Real-Time Unit Industrial Communication Subsystem)。C674X/OMAPL137/8应该是PRUSS,AM335X等应该是PRU-ICSS。这理解不知是否对不对。

    2、关于C编译器

    在 http://downloads.ti.com/codegen/esd/cgt_public_sw/PRU/2.1.3/README.txt 中有如下描述:

    1. Full support of C/C++.
    2. Generates ELF relocatable object files and executables.        
    3. Complete support of the PRU instruction sets (v0, v1, v2, v3).
    4. Constant table accesses from C
    5. Intrinsics for XFER instructions in C
    6. Little and big endian modes
    问题:C6748指令集是V0?还是V1?还是?未找到相关的说明。
    3、关于例程
    在 http://www.ti.com/tool/pru-swpkg 中有三个,确切说应该是两个
    SPRC940.ZIP  是针对 OMAP-L138, C6748, C6746;只有汇编的例程。
    PRU-SWPKG  针对 AM335X等。
    问题:没有看到有针对OMAPL138的C例程,针对PRU-SWPKG适用于OMAP-L138, C6748等?
    4、关于PRU的工作频率,
    在PPT(PRUSS_Training_Slides.pdf)中说其工作频率是CPU的1/2,但在其他地方说是200MHZ,C6748是多少?
    谢谢!
  • tu wolfe 说:
    1、PRU包含了PRUSS(Programmable Real-Time Unit Subsystem)和PRU-ICSS(Programmable Real-Time Unit Industrial Communication Subsystem)。C674X/OMAPL137/8应该是PRUSS,AM335X等应该是PRU-ICSS。这理解不知是否对不对。

    这只是名字上的区别,具体体现在于AM335x的PRU为了工业应用用了Ethercat的网口等。

    tu wolfe 说:
    问题:C6748指令集是V0?还是V1?还是?未找到相关的说明。

    OMAP1x8           - v1

    AM18xx             - v1

    OMAP1x7           - v1

    AM17xx             - v1

    AM33xx             - v3

    AM43xx             - v3

    TMS320C67xx  - v1

    tu wolfe 说:
    3、关于例程
    在 http://www.ti.com/tool/pru-swpkg 中有三个,确切说应该是两个
    SPRC940.ZIP  是针对 OMAP-L138, C6748, C6746;只有汇编的例程。
    PRU-SWPKG  针对 AM335X等。
    问题:没有看到有针对OMAPL138的C例程,针对PRU-SWPKG适用于OMAP-L138, C6748等?

    没有L138的PRU C例程。

    tu wolfe 说:
    4、关于PRU的工作频率,
    在PPT(PRUSS_Training_Slides.pdf)中说其工作频率是CPU的1/2,但在其他地方说是200MHZ,C6748是多少?

    CPU的一半,因为其所用的时钟是PLL0_sysclk2,固定为CPU的一半。

  • 非常感谢!!电脑在国庆前坏了,导致近期都只能看看文档,后期试了再请教。