Error connecting to the target:
Error 0x00000202/-2091
Error during: Memory, OCS,
Device driver: Emulation Connection Loss Detected on Target CPU.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
I/O Port = 240
Board Name: C672x SEEDXDS510PLUS Emulator
Cpu Name: TMS320C672x_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
在3.3上选的672x那个seed xds510plus
或者哪个仿真器支持6726B这个型号