This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6748电源中1.8V电源不正常的问题



我现在在使用C6748这款DSP的时候遇到点供电上的问题,想请教一下大家。
C6748的DDR部分供电的1.8V会变到2.7V,把DSP的1.8V供电断开后,电源芯片输出和DDR供电均为正常1.8V,把DSP的3.3V供电断开后DSP的1.8V供电也是正常的。当1.8V变为2.7V时,DSP整体供电电流会增加,DSP在常温下有时可以正常工作,但低温下就出现无法访问DDR的情况。
DSP的电源中只有DDR部分使用的是1.8V,IO口均使用3.3V,接口使用了EMIF、DDR、SPI和部分GPIO,未使用USB和SATA。
我们最早是在2014年开始使用C6748这款DSP,当时遇到过一次这个问题,更换DSP后就正常了,之后一直都没再出现过这个问题,直到最近又出现了这个问题。出现这个问题的产品的早期批次也没有这个问题,产品的设计都未修改,使用的1.8V和3.3V电源芯片在非C6748平台上也没出过类似问题,所以还是怀疑是DSP本身导致这个问题的出现。
这个问题我们想过很多办法,都没能解决,现在在尝试把去年生产的产品上的DSP拆下来换到出问题的产品上,但由于生产条件的原因可能要很久。。
所以想请教一下大家,希望不吝指教。