你好,我参照mcbsp.c编写了个简单的字符设备,配置DM8168 MCBSP,配置寄存器失败。
写入RCR2寄存器 (0x47000118)的值为0x01后,读取值为0, 设置SPCR2( 0x470000110) 为0xc0, 读取值为0.
读取 XBUFFSTAT(0x470000B4) 的值为0x80
请问还有哪些步骤需要操作,才能正常配置寄存器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tom,
你用DVR RDK提供的mem_rdwr.out工具可以正确写入你在驱动里面配置的寄存器么?如果可以,请检查一下你的驱动。如果不可以,请检查一下mcbsp相关时钟等是否使能/配置。
你好,
我使用mem_rdwr.out工具进行了如下操作,
加载驱动前使用mem_rdwr.out读取
地址 值 寄存器
0x48181400 (08302102) CM_ALWON_L3_SLOW_CLKSTCTRL[12](CLKACTIVITY_MCBSP_AUX_GCLK=0)
0x4818154C (00030000) CM_ALWON_MCBSP_CLKCTRL( MODULEMODE[1-0]=0 IDLEST[17-16]=3)
加载我编写的驱动后,再次使用mem_rdwr.out读取
地址 值 寄存器
0x48181400 (08303102) CM_ALWON_L3_SLOW_CLKSTCTRL[12](CLKACTIVITY_MCBSP_AUX_GCLK=1)
0x4818154C (00000002) CM_ALWON_MCBSP_CLKCTRL( MODULEMODE[1-0]=2 IDLEST[17-16]=0)
按照寄存器说明,是不是表示时钟已经使能?
但是使用mem_rdwr.out对SYSCON(0x47000010)读取值为0x210,与驱动中 SYSCON(0x47000010)写入0x214,读取为0x210。
使用mem_rdwr.out 对0x47000114写入 0xc,写入失败。
请问还有些配置需要操作?
./mem_rdwr.out --rd 47000000 100
0x47000000: EE6477D7
0x47000004: 00000000
0x47000008: 00000000
0x4700000c: 00000000
0x47000010: 00000210
0x47000014: 00000000
0x47000018: 00000000
0x4700001c: 00000000
0x47000020: 00000000
0x47000024: 00000000
0x47000028: 00002000
0x4700002c: 00000001
0x47000030: 00000000
0x47000034: 00000000
0x47000038: 00000000
0x4700003c: 00000000
0x47000040: 00000000
0x47000044: 00000000
0x47000048: 00000000
0x4700004c: 00000000
0x47000050: 00000000
0x47000054: 00000000
0x47000058: 00000000
0x4700005c: 00000000
0x47000060: 00000000
0x47000064: 00000000
0x47000068: 00000000
0x4700006c: 00000000
0x47000070: 00000000
0x47000074: 00000000
0x47000078: 00000000
0x4700007c: 00000036
0x47000080: 00000000
0x47000084: 00000000
0x47000088: 00000000
0x4700008c: 00000000
0x47000090: 00000000
0x47000094: 00000000
0x47000098: 00000000
0x4700009c: 00000000
0x470000a0: 00000112
0x470000a4: 00000000
0x470000a8: 00000000
0x470000ac: 00001008
0x470000b0: 00000808
0x470000b4: 00000080
0x470000b8: 00000000
0x470000bc: 00000084
0x470000c0: 00000000
0x470000c4: 00000000
0x470000c8: 00000000
0x470000cc: 00000000
0x470000d0: 00000000
0x470000d4: 00000000
0x470000d8: 00000000
0x470000dc: 00000000
0x470000e0: 00000000
0x470000e4: 00000000
0x470000e8: 00000000
0x470000ec: 00000000
0x470000f0: 00000000
0x470000f4: 00000000
0x470000f8: 00000000
0x470000fc: 00000000
0x47000100: 00000000
0x47000104: 00000000
0x47000108: 00000000
0x4700010c: 00000000
0x47000110: 00000000
0x47000114: 00000000
0x47000118: 00000000
0x4700011c: 00000000
0x47000120: 00000000
0x47000124: 00000000
0x47000128: 00000000
0x4700012c: 00000000
0x47000130: 00000000
0x47000134: 00000000
0x47000138: 00000000
0x4700013c: 00000000
0x47000140: 00000000
0x47000144: 00000000
0x47000148: 00000000
0x4700014c: 00000000
0x47000150: 00000000
0x47000154: 00000000
0x47000158: 00000000
0x4700015c: 00000000
0x47000160: 00000000
0x47000164: 00000000
0x47000168: 00000000
0x4700016c: 00000000
0x47000170: 00000000
0x47000174: 00000000
0x47000178: 00000000
0x4700017c: 00000000
0x47000180: 00000000
0x47000184: 00000000
0x47000188: 00000000
0x4700018c: 00000000
你好,
你是否使用的是ti网站上最新的TRM?
为什么要0x47000114写入0xc?这个寄存器的bit2/3都是状态值,而且bit2是只读的?
114h SPCR1_REG McBSP Serial Port Control Register 1
3 RSYNCERR Receive Synchronization Error.
(Writing 0 to this bit clear the legacy receive interrupt if asserted due to RSYNCERROR condition).
0 No synchronization error.
1 Synchronization error detected by McBSP.
2 RFULL Receive Shift Register (RSR [1,2]) Full.
0 RB is not in overrun condition.
1 DRR is not read, RB is full and RSR is also full with new word.
也确认一下mcbsp的时钟源是否有选择:
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/468960
你好:
我寄存器基值改成0x47000100,通过poll模式已经可以接受数据,
如下为寄存器配置值
SYSCON:0x00000214
DRR: 0x00000055
DXR: 0x00000000
SPCR2: 0x00000203
SPCR1: 0x00000007
RCR2: 0x00000000
RCR1: 0x00000000
XCR2: 0x00000001
XCR1: 0x00000000
SRGR2: 0x0000000f
SRGR1: 0x00000101
MCR2: 0x00000000
MCR1: 0x00000000
PCR0: 0x00000001
RCERA: 0x00000000
RCERB: 0x00000000
PCR: 0x00000001
THRSH2: 0x00000000
THRSH1: 0x00000007
XCCR: 0x00000000
RCCR: 0x00000008
XBUFFSTAT: 0x00000080
RBUFFSTAT: 0x00000080
WAKEUPEN: 0x00000408
但是edma处理没有正常工作。RRDY位已经位1,TRM上mcbsp IRQ位86 ,edma 的MCBSP_RX 位15,均已申请。
以为edma相关代码,请问设置上是否有问题?
dev->rx_dma_buf = kzalloc(DMA_BLOCK_SIZE, GFP_KERNEL | GFP_DMA);
if (!dev->rx_dma_buf){
dev_err(dev->dev, "McBSP RX kzalloc() failed\n");
return -ENOMEM;
}
r = edma_alloc_channel(dev->rx_dma_sync, ti816x_mcbsp_rx_edma_callback, dev, EVENTQ_0);
if(r<0){
dev_err(dev->dev,"Unable to request DMA channel for MCBSP RX\n");
goto error_channel;
}
dev->rx_dma_channel = r;
printk(KERN_INFO "McBSP RX EDMA on channel %d\n",dev->rx_dma_channel);
dev->rx_dma_addr = dma_map_single(dev->dev, dev->rx_dma_buf, DMA_BLOCK_SIZE,DMA_FROM_DEVICE);
if (dma_mapping_error(dev->dev, dev->rx_dma_addr)) {
dev_err(dev->dev, "Couldn't DMA map a %d bytes RX buffer\n",DMA_BLOCK_SIZE);
if (dev->rx_dma_buf != NULL)
dma_unmap_single(NULL, dev->rx_dma_addr, DMA_BLOCK_SIZE, DMA_FROM_DEVICE);
goto error_map;
}
edma_set_transfer_params(dev->rx_dma_channel,TI816x_DMA_DATA_TYPE_S32, 1, 1, 0, ASYNC);
edma_set_src(dev->rx_dma_channel,dev->rx_reg, INCR, W8BIT);
edma_set_dest(dev->rx_dma_channel,dev->rx_dma_addr, INCR, W8BIT);
edma_set_src_index(dev->rx_dma_channel, 0, 0);
edma_set_dest_index(dev->rx_dma_channel,TI816x_DMA_DATA_TYPE_S8, 0);
edma_start(dev->rx_dma_channel);
你好:
我EDMA 参数设置如下,B_CNT = 1;
/* set to A-synchronized mode acnt*bcnt triger edma*/
param.opt = TCINTEN | // Transfer complete interrupt is enabled
EDMA_TCC(channel) | // Transfer complete code
(0 << 8) | // FWID FIFO width is 8-bit
1; // Source address mode. Constant addressing (CONST) mode
param.src = 0x47000000; //TI816x_MCBSP_BASE + MCBSP_DRR ;
param.a_b_cnt = (B_CNT << 16) | 0x1;
param.dst = buf_phyaddr;
param.src_dst_bidx = 0x00010000; // src_inx = 0 fix src register
param.link_bcntrld = (B_CNT << 16) | 0xFFFF ;
param.src_dst_cidx = 0 ;
param.ccnt = 1;
但是 mcbsp rccr 寄存器设置如下,RDMAEN 置0,按照TRM的意思,应该是关闭DMA请求,但是配置EDMA参数,edma_start()后,rx_edma_callback还是能进入。请问是那部分寄存器设置有问题?还是EDMA配置有问题?
//RCCR_RFULL_CYCLE;
你好,
我希望使用EDMA来搬移McBSP的数据。McBSP做salve模式,Master 为FPGA。
但是在配置完McBSP寄存器和EDMA之后,无论FPGA是否发送数据,EDMA的rx_dma_callback 函数都能进入,而且状态为DMA_COMPLETED。
这个很奇怪,所以我试着RDMAEN 置0,发现还能触发EDMA工作。
还有一个疑问是:在调用完edma_start()后rx_dma_callback进入后,不会再次进入了。
所以这个现象是EDMA配置有问题还是McBSP寄存器配置的问题。
McBSP寄存器参数配置如下:
mcbsp_config.rcr1 = RCR1_RFRLEN1(TI81XX_MCBSP_WORD_8) |
RCR1_RWDLEN1(TI81XX_MCBSP_WORD_8);
mcbsp_config.xcr1 = XCR1_XFRLEN1(TI81XX_MCBSP_WORD_8) |
XCR1_XWDLEN1(TI81XX_MCBSP_WORD_8);
mcbsp_config.rcr2 = RCR2_RDATDLY(1);
mcbsp_config.xcr2 = XCR2_XDATDLY(1);
mcbsp_config.pcr0 = PCR_CLKRP;
mcbsp_config.srgr1 = SRGR1_FWID(1) |
SRGR1_CLKGDV(1) ;
mcbsp_config.srgr2 = SRGR2_FPER(16);
mcbsp_config.spcr1 = SPCR1_RINTM(0);
mcbsp_config.spcr2 = SPCR2_FREE;
mcbsp_config.rccr = RCCR_RDMAEN;