自己做的板子,SDK7.0的Linux 3.12如何才能正常使用
已经屏蔽了UBOOT中EEPROM ID验证部分,但是Linux kernel启动不了
如下
UBOOT好像可以正常启动了
U-Boot SPL 2013.10-00189-g78d8ebd-dirty (Oct 11 2016 - 11:05:59)
reading args
spl: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2013.10-00189-g78d8ebd-dirty (Oct 11 2016 - 11:05:59)
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Error - No Valid Environment Area found
*** Warning - bad CRC, using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
Could not get PHY for cpsw: addr 0
cpsw, usb_ether
下面是kernel启动部分,停在Starting kernel ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3ed470 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8f31f000, end 8f32c25b ... OK
Starting kernel ...
Linux部分要做什么修改才能正常启动?