This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713B作为SPI从机,rrdy置位问题



1. 问题:C6713B作为从机,通过McBSP与STM32F407进行SPI通信,C6713B在接收SPI数据时,McBSP的rrdy(SPCR)不会自动置1。通过示波器查看,STM32发出的时钟和数据都是正常的。

2.  原理图设计:

(1)DSP端接口

(2)STM32端接口

其中PA5,PA6接口复用了(测试时STM32只有SPI程序)

3. 程序

(1)C6713B程序

配置McBSP

void ConfigMcbsp(MCBSP_Handle *hMcbsp_ch0) {

*hMcbsp_ch0 = MCBSP_open(MCBSP_DEV1, MCBSP_OPEN_RESET);

/* create a config structure for digital SPI slave mode */

static MCBSP_Config ConfigSPISlave = {

MCBSP_SPCR_RMK(

        MCBSP_SPCR_FREE_YES,

        MCBSP_SPCR_SOFT_YES,

   MCBSP_SPCR_FRST_YES

   MCBSP_SPCR_GRST_YES,

        MCBSP_SPCR_XINTM_XRDY,

        MCBSP_SPCR_XSYNCERR_NO,

        MCBSP_SPCR_XRST_YES,

        MCBSP_SPCR_DLB_OFF,

        MCBSP_SPCR_RJUST_RZF,

        MCBSP_SPCR_CLKSTP_NODELAY,

        MCBSP_SPCR_DXENA_OFF,

        MCBSP_SPCR_RINTM_RRDY,

        MCBSP_SPCR_RSYNCERR_NO,

        MCBSP_SPCR_RRST_YES

 ),

  /*  Receive Control Register (RCR) */

MCBSP_RCR_RMK(

   MCBSP_RCR_RPHASE_SINGLE,

        MCBSP_RCR_RFRLEN2_OF(0),

        MCBSP_RCR_RWDLEN2_16BIT,

        MCBSP_RCR_RCOMPAND_MSB,

        MCBSP_RCR_RFIG_NO,

        MCBSP_RCR_RDATDLY_0BIT,

        MCBSP_RCR_RFRLEN1_OF(0),

        MCBSP_RCR_RWDLEN1_16BIT,

        MCBSP_RCR_RWDREVRS_DISABLE

  ),

  /* Transmit Control Register (XCR) */

MCBSP_XCR_RMK(

        MCBSP_XCR_XPHASE_SINGLE,

        MCBSP_XCR_XFRLEN2_OF(0),

        MCBSP_XCR_XWDLEN2_8BIT,

        MCBSP_XCR_XCOMPAND_MSB,

        MCBSP_XCR_XFIG_YES,

        MCBSP_XCR_XDATDLY_0BIT,

        MCBSP_XCR_XFRLEN1_OF(0),

        MCBSP_XCR_XWDLEN1_32BIT,

   MCBSP_XCR_XWDREVRS_DISABLE

  ),

  /*serial port sample rate generator register(SRGR) */

MCBSP_SRGR_RMK(

        MCBSP_SRGR_GSYNC_FREE,

        MCBSP_SRGR_CLKSP_RISING,

        MCBSP_SRGR_CLKSM_INTERNAL,

        MCBSP_SRGR_FSGM_DXR2XSR,

        MCBSP_SRGR_FPER_OF(0),

        MCBSP_SRGR_FWID_OF(0),

        MCBSP_SRGR_CLKGDV_OF(1)

  ),

  MCBSP_MCR_DEFAULT,

  MCBSP_RCER_DEFAULT,

  MCBSP_XCER_DEFAULT,

  /* serial port pin control register(PCR) */

MCBSP_PCR_RMK(

        MCBSP_PCR_XIOEN_SP,

        MCBSP_PCR_RIOEN_SP,

        MCBSP_PCR_FSXM_EXTERNAL,

        MCBSP_PCR_FSRM_EXTERNAL,

        MCBSP_PCR_CLKXM_INPUT,

        MCBSP_PCR_CLKRM_INPUT,

        MCBSP_PCR_CLKSSTAT_0,

        MCBSP_PCR_DXSTAT_0,

        MCBSP_PCR_FSXP_ACTIVELOW,

        MCBSP_PCR_FSRP_ACTIVELOW,

        MCBSP_PCR_CLKXP_FALLING,

        MCBSP_PCR_CLKRP_FALLING

  )

};

MCBSP_config(*hMcbsp_ch0, &ConfigSPISlave);

/* ---------------------------------------------------------------------------*/

void StartMcbsp(MCBSP_Handle *hMcbsp_ch0) {

int i;

 

MCBSP_enableSrgr(*hMcbsp_ch0);

 

for(i = 5; i > 0; i--);

MCBSP_enableFsync(*hMcbsp_ch0);

MCBSP_enableRcv(*hMcbsp_ch0);

MCBSP_enableXmt(*hMcbsp_ch0);

 

for(i = 5; i > 0; i--);

}

Main()函数

void main() {

       int i;

 

       CSL_init();

 

       ConfigMcbsp(&hMcbsp_ch0);

 

       IRQ_setVecs(vectors);

 

       IRQ_globalEnable();

 

       IRQ_nmiEnable();

 

       for(i = 0; i < 32; i++) {

              IRQ_disable(i);

              IRQ_clear(i);

       }

 

 

       IRQ_map(IRQ_EVT_RINT1, 4);

 

       IRQ_reset(IRQ_EVT_RINT1);

 

       IRQ_enable(IRQ_EVT_RINT1);

 

       StartMcbsp(&hMcbsp_ch0);

 

       MCBSP_write(hMcbsp_ch0, 0x0000e40a);

       while(!MCBSP_rrdy(hMcbsp_ch0));

       data = MCBSP_read(hMcbsp_ch0);

      

       while(1) {

       }

}

 

中断函数

interrupt void SPIEventIsr(void) {

       data = MCBSP_read(hMcbsp_ch0);

}

 

中断向量配置

*------------------------------------------------------------------------------

* Global symbols defined here and exported out of this file

*------------------------------------------------------------------------------

   .global _vectors

   .global _c_int00

   .global _vector1

   .global _vector2

   .global _vector3

   .global _SPIEventIsr ; Hookup the SPI ISR in main()

   .global _vector5

   .global _vector6

   .global _vector7

   .global _vector8

   .global _vector9  

   .global _vector10

   .global _vector11  

   .global _vector12 

   .global _vector13  

   .global _vector14

   .global _vector15

 

*------------------------------------------------------------------------------

* This is the actual interrupt service table (IST). It is properly aligned and

* is located in the subsection .text:vecs. This means if you don't explicitly

* specify this section in your linker command file, it will default and link

* into the .text section. Remember to set the ISTP register to point to this

* table.

*------------------------------------------------------------------------------

 .sect ".text:vecs"

 .align 1024

 

_vectors:

_vector0:   VEC_ENTRY _c_int00    ;RESET

_vector1:   VEC_ENTRY _vec_dummy  ;NMI

_vector2:   VEC_ENTRY _vec_dummy  ;RSVD

_vector3:   VEC_ENTRY _vec_dummy

_vector4:   VEC_ENTRY _SPIEventIsr

_vector5:   VEC_ENTRY _vec_dummy

_vector6:   VEC_ENTRY _vec_dummy

_vector7:   VEC_ENTRY _vec_dummy

_vector8:   VEC_ENTRY _vec_dummy

_vector9:   VEC_ENTRY _vec_dummy

_vector10:  VEC_ENTRY _vec_dummy

_vector11:  VEC_ENTRY _vec_dummy

_vector12:  VEC_ENTRY _vec_dummy

_vector13:  VEC_ENTRY _vec_dummy

_vector14:  VEC_ENTRY _vec_dummy

_vector15:  VEC_ENTRY _vec_dummy

(2)STM32程序

SPI配置

void SPI1_Init(void) {

       GPIO_InitTypeDef GPIO_InitStructure;

       SPI_InitTypeDef SPI_InitStructure;

 

       RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

       RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

 

       GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

       GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;  //复用功能

       GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;  //推挽输出

       GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

       GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;  //上拉

       GPIO_Init(GPIOA, &GPIO_InitStructure);

 

       GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

       GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

       GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

       GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

       GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

       GPIO_Init(GPIOA, &GPIO_InitStructure);

 

       GPIO_ResetBits(GPIOA, GPIO_Pin_4);

 

       GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);  //PA5复用为SPI1

       GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);

       GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);

 

       RCC_APB2PeriphResetCmd(RCC_APB2Periph_SPI1, ENABLE);  //复位SPI1

       RCC_APB2PeriphResetCmd(RCC_APB2Periph_SPI1, DISABLE);  //停止复位SPI1

 

       SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;  //设置双向模式

       SPI_InitStructure.SPI_Mode = SPI_Mode_Master;  //SPI主模式

       SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; //16位帧结构

       SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;  //时钟极性

       SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;  //时钟相位

       SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;  //NSS信号由SSI位控制

       SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256;  //256分频

       SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;  //数据位从MSB位开始

       SPI_InitStructure.SPI_CRCPolynomial = 7;  //CRC值计算的多项式

       SPI_Init(SPI1, &SPI_InitStructure);

 

       SPI_Cmd(SPI1, ENABLE);  //使能SPI外设

 

       SPI1_ReadWriteByte(0xffff);  //启动传输

}

 

u16 SPI1_ReadWriteByte(u16 txdata) {

       while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET) {}  //等待发送区空

       SPI_I2S_SendData(SPI1, txdata);

 

       while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET) {}  //等待接收完一个byte

      

       return SPI_I2S_ReceiveData(SPI1);  //返回SPI1最近接收到的数据

}           

 

Main()函数

int main() {

             u8 i;

             volatile u16 high16bits = 0;

             volatile u16 low16bits = 0;

             volatile u16 temp;

 

             SPI1_Init();

             DelayInit();

             for(i = 0; i < RXDATA_SIZE; i++) xdata[i] = i;

 

             Delayms(500);

            

             while(1) {

              for(i = 0; i < RXDATA_SIZE; i++) {  //每次发32个数据

                     Delayus(4);

                     GPIO_SetBits(GPIOA, GPIO_Pin_4);

                     Delayus(4);

                     GPIO_ResetBits(GPIOA, GPIO_Pin_4);

                     Delayus(4);

                     high16bits = SPI1_ReadWriteByte(xdata[i]) ;

              }

             }

}

麻烦老师帮忙看一下问题,如有结果烦请尽快告知,谢谢!第一次发帖求助,如有不规范的地方还请多多指教。