This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368+TVP7002是否可以实现两路VGA采集 分辨率最高到1920x1080@60Hz?

Other Parts Discussed in Thread: TVP7002

如题,之前没接触过视频采集这方面,现在要做一个采集两路VGA的方案,不知道用DM368+TVP7002是否可以?

TVP7002是否可以接两路VGA信号那》?

  • Alex,

    不可。

    TVP7002只能输入单路VGA (PC)信号。

    DM368的采集并口,最高时钟支持120Mhz,一路1080p60也无法接入。

    如果你要接入两路1080p60,而且要编码,你可以看看DM816x。如果只是接入,不编码,你可以看看DM385.

  • 我看TVP7002的datasheet,是三组RGB模拟引脚输入,为什么只能输入单路VGA那?那剩下的两组模拟引脚输入干什么用呢?

    我觉得应该是这样,如果想采集的VGA信号是1080P60的话TVP7002只支持一路输入,因为TVP7002的时钟最大是165M,165M只能传输一路1080P60信号的数据量。如果采集的VGA信号不是1080P60,比如是800*400或者更低是不是就可以输入两路或者三路,不知道是不是这样?

  • 你好,

    你看看下面的帖子里的信息:

    https://e2e.ti.com/support/data_converters/videoconverters/f/376/p/112694/399466#399466