新买的AM437x IDK 开发套件,里面出厂时是否有烧录电机驱动应用程序,能够在拿回来时直接连接电机进行测试查看效果?看官方“AM437x Single-Chip Motor-Control Design Guide”手册里写着该开发板可以直接连接电机实现运转,不知该测试该如何进行?希望了解的大侠指点一二。。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该是下载industry sysbios SDK:
http://processors.wiki.ti.com/index.php?title=SYSBIOS_Industrial_SDK_Getting_Started_Guide
http://processors.wiki.ti.com/index.php/SYSBIOS_Industrial_SDK_02.01.01_Release_Notes
http://processors.wiki.ti.com/index.php/SYSBIOS_Industrial_SDK_02.01.01_User_Guide#Motor_Control
我们买了两块新开发板,试了一下,有一块能通过xds100V2连上,有一块却不行,出现如下错误提示,麻烦您帮忙看下是什么原因。谢谢!
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\LY\AppData\Local\TEXASI~1\CCS\ti\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.
The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
你好!是win7. 好的。
昨天我在下载TI例程是又碰到一个问题,错误提示如下:
CortxA9: Trouble Writing Memory Block at 0x80000000 on Page 0 of Length 0x7ff0: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.83.1)
CortxA9: File Loader: Verification failed: Target failed to write 0x80000000
CortxA9: GEL: File: C:\ti\motor control\motor control.out: Load failed.
没法把.out文件下进去,不知有没有碰到过这个问题?提示访问不了存储设备。