This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tci6638 arm linux 如何关闭phy芯片



我们有一块单板使用了tci6638,与EVM板不同的是,GE网口eth0没有接phy,而是直接与板上switch通过sgmii直连。

现在想在arm上运行sdk(ti-processor-sdk-linux-k2e-evm-03.00.00.04-Linux-x86-Install.bin)上的linux系统。

系统已经烧录成功并且能够运行,但是网口无法工作。

查看dmesg信息,发现

[ 1.809078] libphy: Fixed MDIO Bus: probed
[ 2.315939] ti,keystone-serdes 232a000.phy: lane 1 wait rx valid failed: -110
[ 2.323101] ti,keystone-serdes 232a000.phy: serdes lanes enable failed: -110
[ 2.330186] phy phy-232a000.phy.0: phy init failed --> -110
[ 2.335778] netcp-1.0 2620110.netcp: Probe of module(netcp-gbe) failed with -110
[ 2.343219] netcp-1.0 2620110.netcp: module(netcp-xgbe) not used for device

请教各位高手,针对这个情况,linux系统需要做什么修改,网口才能正常工作?