This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138使用SATA3接口硬盘问题

Other Parts Discussed in Thread: OMAP-L138

一、关于OMAPL138使用SATA3接口硬盘问题

速度不需要达到SATA3,在SATA1/SATA2的速度下能稳定即可

1、目前使用SATA3接口硬盘,会出现连不上硬盘的情况

CPU: OMAPL138 内核:linux-3.3

连不上硬盘时,出现的错误日志

[   29.761498] ata1: exception Emask 0x10 SAct 0x0 SErr 0x4050002 action 0xe frozen

[   29.769002] ata1: irq_stat 0x00000040, connection status changed

[   29.777109] ata1: SError: { RecovComm PHYRdyChg CommWake DevExch }

[   29.784692] ata1: hard resetting link

[   32.009548] ata1: SATA link down (SStatus 1 SControl 300)

[   32.015088] ata1: EH complete

2、关于文档OMAP-L138 C6000 DSP+ARM Processor Technical Reference Manual

文档中的一些SATA相关寄存器的设置,不明白其实际作用。SATA相关寄存器主要有:

P0CMD.CPD、P0CMD.MPSP、P0CMD.ESP、P0CMD.HPSP、P0PHYCR.RXCDR,希望能更详细的说明其作用,并能够提供更多SATA相关文档。

3、TI目前关于OMAPL138芯片使用SATA3接口硬盘有没有解决方案?

4、关于OMAPL138芯片USB的稳定性

如使用USB转SATA的方案,7*24小时的使用,USB稳定性方面是否可靠?