请问我现在在DM385(就是appro那个参考设计)上配置ar0331的wdr模式,
ipnc rdk 版本是V3.8.0,开启WDR_ON后发现ar0331不输出东西。
在issdrv_ar0331Api.c 中的Transplant_DRV_imgsSetRegs函数中加打印发现
wdr 模式下的i2c配置sensor sequencer时有失败的情况,如果把配置sequencer的代码全部注释掉
就能够采到图像了
请问这里i2c 写失败正常吗?这个sequencer 配置是不是必须的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Du Jun,
I2C需要配置sensor输出WDR的RAW数据,这样DM385才能正确输出.
感谢回复
您说的“I2C需要配置sensor输出WDR的RAW数据,这样DM385才能正确输出”
我这边就是在进行i2c对sensor进行配置的的时候有写失败的情况,然后cameralink的打印显示采不到东西,
那些ar0331的i2c配置我没有改过,就是ipnc rdk 3.8.0原版的,打印发现
wdr 模式下的i2c配置sensor sequencer时有失败的情况,如果把配置sequencer的代码全部注释掉
就能够采到图像了,请问sequencer的配置是必须的吗?
jun du 说:请问正常情况下我只要Rule.make里开启WDR然后make all 这个ar0331的wdr模式就应该好使了?
SENSOR_BOARD_VENDOR和HARDWARE_REVISION是否配置正确?
Chris Meng 说:请问正常情况下我只要Rule.make里开启WDR然后make all 这个ar0331的wdr模式就应该好使了?SENSOR_BOARD_VENDOR和HARDWARE_REVISION是否配置正确?
[/quote]
您好,SENSOR_BOARD_VENDOR确认了是Leopard Imaging Board上面写着Li-CAM-AR0331-1.8_v1.0,这个之前写错了
HARDWARE_REVISION 我问了下我们的硬件应该是rev2,1.8v的
按您的提示改过来后重试还是i2c写失败,现在进一步详细打印发现写失败的寄存器似乎总是固定几个,发生在刚开始的sequencer配置时
[m3vpss ] 852: SYSTEM : Device Init in progress DONE !!!
[m3vpss ] I2C write Error,index:1,301a,10d8
[m3vpss ] I2C write Error,index:51,3086,0d57
[m3vpss ] I2C write Error,index:83,3086,fa45
[m3vpss ] I2C write Error,index:84,3086,a017
[m3vpss ] 913: SYSTEM : System VPSS Init Done !!麻烦您再帮看下
Du Jun,
能否再确认一下硬件版本?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/p/63824/174819.aspx
请看一下机器侧边有RS485信号输入的那排注释里面GND是几?如果GND是5就是REV2的机器,GND是3就是REV1的机器。
301a的寄存器是复位寄存器,不应该不能否复位啊。
Chris Meng 说:Du Jun,
能否再确认一下硬件版本?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/p/63824/174819.aspx
请看一下机器侧边有RS485信号输入的那排注释里面GND是几?如果GND是5就是REV2的机器,GND是3就是REV1的机器。
301a的寄存器是复位寄存器,不应该不能否复位啊。
您说的那个是在外壳上吗,我手里这个没壳了。但是
1,这板子我拿到后uboot和kernel打印都有DM385_IPNC_3.50.00的字样,按您在链接帖子说的ipnc rdk 3.5支持的是rev1,我这个就是rev1了?
2,另外我把那段有错的sequencer寄存器全部注释掉可以出图像,这样对wdr对有影响没,新手不知道不太懂,sequencer ar0331的手册上就没提啊,我能接着这么调吗?