This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

多核dspC6670/1/2/4/8是否完全兼容?



请问多核dspC6670/1/2/4/8是否完全兼容?可以相互替换?

  • 你好,dspC6670/1/2/4/8是互相兼容的。

  • 1. 6670的每个core内部memory是1M,6671/2/4/8每个core内部memory是512K,使用时要注意。6670 shared memory 是2M,6671/2/4/8应该是4M。

    2.6670有些无线加速器,6671/2/4/8则没有这些无线加速器

    3.6671/2/4/8应该是有EMIF16接口的,而6670没有该接口

    4.6670有AIF2接口,6671/2/4/8没有,其他的东西都是一样的。

    6671/2/4/8的管脚应该是兼容的,可以互相替换。但是功耗不一样,这点做热设计需要注意。