本人将DM8127 管脚(AE6 AF5)配置成uart4模式。当前发送可以,但是接收始终无法得到,uart1,2已经调试通。 datasheet中描述uart3,4,5支持高速模式。请问和这个有关系吗?除了配置mux复用为uart4,还有其他什么需要配置的? 我是用的ipnc_rdk3.5
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人将DM8127 管脚(AE6 AF5)配置成uart4模式。当前发送可以,但是接收始终无法得到,uart1,2已经调试通。 datasheet中描述uart3,4,5支持高速模式。请问和这个有关系吗?除了配置mux复用为uart4,还有其他什么需要配置的? 我是用的ipnc_rdk3.5
Guo Xingxian,
请检查一下是否有其他引脚也配置成了UART4的RX。
之前有客户配置了两个引脚都是同一个RX功能,然后接收就有问题。