This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:Unable to read "boot.scr" from mmc 0:1



一直产品都存在这个隐患,可能在某个时候就会出现这个问题
有没有解决方案啊?
U-Boot 2009.11 ( 9月 15 2015 - 04:52:33)
 
I2C:   ready
DRAM:  128 MB
NAND:  512 MiB
MMC:   davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
*** Warning - bad CRC or NAND, using default environment
 
In:    serial
Out:   serial
Err:   serial
ARM    Clock : 300000000 Hz
DDR    Clock : 150000000 Hz
EMIFA  CLock : 150000000 Hz
DSP    Clock : 300000000 Hz
ASYNC3 Clock : 150000000 Hz
Enet  config : 0
MMC 0 Enable : 0
Mach_Number: 2650
Resetting ethernet phy
hellowode++++++++++++++++0+++++++++++++++++!
hellowode++++++++++++++++1+++++++++++++++++!
hellowode++++++++++++++++2+++++++++++++++++!
Resetting Beep Pin_hellowode!
Set Ethernet MAC addrress!
00:50:c2:e6:77:22
Net:   Ethernet PHY: GENERIC @ 0x1f [0x80000000]
 
Hit any key to stop autoboot:  0
 
Loading from nand0, offset 0x120000
** Unknown image type
reading boot.scr
 
** Unable to read "boot.scr" from mmc 0:1 **
reading uImage
 
** Unable to read "uImage" from mmc 0:1 **
8192 KiB M25P64 at 0:0 is now current device
Wrong Image Format for bootm command
ERROR: can't get kernel image!