Other Parts Discussed in Thread: TMS320C6416
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\ADMINI~1.GOS\AppData\Local\.TI\ 693494126\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product. This utility will load the adapter 'seedjca8990isa.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is not generated by TI's USCIF driver or utilities.
The USCIF driver and utilities use the range from -2 down to -999
The value is '+134' (0x00000086). The title is unavailable. The explanation is unavailable.
[End]