群内的大神们:
你们好! 我用的是基于8127芯片, ipnc-rdk 3.8 ,在m3vpss核上用到EDMA时遇到了问题,具体用到的EDMA接口函数如下:
void DM81XX_EDMA3_setParams(int chId, int dmaQueue, unsigned int srcAddr, unsigned int dstAddr, unsigned short edmaWidth,
unsigned short edmaHeight, short srcLineOffset, short dstLineOffset);
void DM81XX_EDMA3_triggerTransfer(int chId);
由于需要,我在操作每帧数据时大概会调用上述接口130次左右,我使用的是chId=12, dmaQueue=0,
能够正常运行一段时间(从10分钟到1个小时不等), 随后就卡在这个地方了,我想咨询的是:
1)这个EDMA调用频率不能太频繁吗?大概什么样的频率能正常工作?
2)我在m3vpss中使用,chId这个值的范围是多少的? 还是dmaQueue的范围是多少呢?
3)如果EDMA不能调用太频繁,在m3vpss核上进行内存拷贝,我还能采取什么方式能比较快的完成(memcpy太慢)?
先谢谢啦,困扰了好多天,请指点...