This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X StarterWare GA release (02.00.00.07) 发布了!!!!



·         The release contains
o   StarterWare user Boot Loader and Standalone Applications running from DDR
o   Support for various boots modes (MMCSD, UART, SPI (EVM only), NAND(EVM only))
o   USB library (stack ported from StellarisWare)
o   Graphics Library (ported from StellarisWare)
o   LwIP stack to updated to latest version (1.4.0)
o   Driver APIs for the peripherals/devices: MMC/SD, EMAC, MDIO, USB (CDC, Custom Bulk & MSC), DMTimer, EDMA, GPIO, HSI2C, RTC, McSPI, Raster, McASP, Watchdog timer, TSC_ADC, CAN, EHRPWM.
o   AM335x EVM-SK
·         Sample Applications for peripheral like GPIO, I2C, RTC, LCD, Timer, McASP, Ethernet, MMC/SD, TouchScreen, ADC, UART, USB
·         Out-of-box demo application which demonstrates the peripherals RTC, Raster LCD, Timer, McASP, Ethernet, MMC/SD, TouchScreen, UART, eCAP, I2C, GPIO, Power Management(DS0) and DVFS (for MPU). The OOB has Matrix menu (LCD / Web page based) for driving the out-of-box demo example.
·         Maze Game and grlib_demo application examples to demonstrate graphics library capabilities.
·         Tested on AM335X v1.2B EVM-SK.
o   AM335x Beta EVM
·         Sample Applications for peripheral like GPIO, I2C, RTC, SPI, LCD, Timer, McASP, Ethernet, MMC/SD, TouchScreen, NAND, ADC, UART, EHRPWM, USB.
·         Out-of-box demo application which demonstrates the peripherals RTC, Raster LCD, Timer, McASP, Ethernet, MMC/SD, TouchScreen, UART, eCAP, I2C, GPIO, Power Management(DS1, DS0) and DVFS (for MPU). The OOB has Matrix menu (LCD / Web page based) for driving the out-of-box demo example.
·         Maze Game and grlib_demo application examples to demonstrate graphics library capabilities.
·         Tested on AM335X v1.1A EVM.
o   Beaglebone support
·         Sample Applications for peripherals like Ethernet, GPIO, MMC/SD, HSI2C, RTC, Timer, UART,watchdog timer, cache/MMU, USB
·         Out-of-box demo application which demonstrates peripherals like Ethernet, GPIO, MMC/SD, RTC, Timer, UART. The OOB has Matrix menu (web page based) for driving demo example.
·         Tested on Beaglebone A3 board (AM335X)
·         Tool chain Support:
o   TI TMS470 ARM tools (Release package includes pre-built sample application binaries built using TMS470)
o   GCC (Code sourcery Lite arm-2009q1-161-arm-none-eabi)
o   IAR Embedded Workbench for ARM 6.30.7 (loading and debugging supported with XDS 100)
 
Release (02.00.00.07) links:
·         Kindly refer release documents for detailed information 
·         Installer package is available at this link (external download link with Auto screen approval process)
·         Link to documents on external wiki
·         To tryout a quick demo refer quick start guide