This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

多片C6678设计配置信号线共享



大家好,

打算做一个6U板子,放6片C6678。有些问题不太确定,来请教一下。

1. 为了节省FPGA用于配置C6678的引脚,比如FPGA控C6678的BootMode Pin(就是GPIO)、各种RESET/CORESEL信号等等,如果用FPGA的一个信号,PCB上直接分到6片C6678是否可行?比如FPGA一个引脚拉出来,分叉给6片C6678的GPIO0。这样的话,需不需要buffer?

2. 如1做法,会使得FPGA控制6片C6678同时Boot,这样还需要其他的考量吗?

3.因为C6678只有一个HyperLink通道,HyperLink能否分拆成2个X2 Lane,使得这一个C6678跟其他两个C6678互联?HyperLink还需要一些FLOW CONTROL等信号,是不是就没法这么做?

谢谢!