McFW中的DEI和DEIH有什么区别?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DEI_H
The DEI_H (High Quality De-interlacer) is primarily used to convert interlaced video source material to progressive
form. This particular module incorporates features such as Temporal Noise Reduction, 4 and 5 field motion detection and very fine edge detection capabilities to produce a very high quality deinterlaced output.
DEI
The DEI (De-interlacer) is primarily used to convert interlaced video source material to progressive form. This
particular module is a reduced feature set of the DEI_H module, in that in does not perform Temporal Noise
Reduction and is limited to 4 field motion detection. It performs edge directed interpolation, but utilizes a simpler
(and smaller) algorithm compared to the DEI_H module.