This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何配置PA接收arp的包?



目前在调试PA的emacexample,已经调通了,可以向PC发送和接收UDP数据包。但是例程中PA的配置是中添加了mac地址,IP地址和port的条目。

因为我后期想添加协议栈,所以我想请问如何添加条目,可以让其接收到PC发送的arp请求包?

  • In response to your ARP question. Assuming that you want to forward all ARP requests (regardless of the source MAC ADDR) to a unique queue you only need to call the Pa_addMac function with the struct below ,ethertype set to 0x0806 (for the ARP ethertype). The rest is don't care.

     

    typedef struct {

    paMacAddr_t  src;  //Source MAC address

    paMacAddr_t   dst;  //destination MAC addr

    unit16_t   vlan; //VLAN tage VID field, 12 lsbs

    uint16_t  ethertype;   //ethertype field

    unit32_t  mplsTag;     

    uint16_t inport;  //input EMAC port number as specfied by the EMAC port

    } paEthInfo_t ;

     

    So, for the matchRoute you can use any flowID you want, you just need to set the queue to the unique one you want the packets to be forwarded to. If you have a separate FDQ or pool of descriptors, you can just set the flowID to the one desired. This will forward all the packets with the ARP ethertype (0x0806) to the dest queue you specified using the flow you want.