This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713: Warning: CPU:Interrupt No. 15 dropped, an earlier interrupt is pending to be taken



运行c6713的edma例程(系统自带的),出现如下错误:

           控制台隔一个定时器定时的时间就会显示一行如下信息:

           TMS320C6713: Warning: CPU:Interrupt No. 15 dropped, an earlier interrupt is pending to be taken  

  • 请问用的是哪个版本的ccs? 是用simulator还是emulator?是哪个edma例程?

  •             你好,谢谢您的耐心解答!!!问题已经解决,原因是没有加载正确的simulator。。。

    还有一个问题想请教您:

                 问题描述:

                                    现在c6713仿真edma已经成功了。我的最终目的是仿真dm8168的edma功能,但是ti并没有提供

                                    dm8168的simulator,而dm8168板子上的dsp核心是c6748,所以我打算用c6748的simulator来

                                    仿真效果。

                 疑惑:

                                   ti给c6748提供的是cslr而不是csl,cslr中并没有提供像DAT_open()一样的EDMA传输接口,如果我

                                   直接去操作寄存器,显得十分麻烦。那么cslr中又没有提供类似的函数直接调用呢(像DAT_open()一样)。

                                   另外,大概看了下cslr中的结构,好像使用的是edma3去实现edma功能的,cslr中没有提供像csl中那么详细

                                  的例子,我该怎么着手呢?这方面有什么例子参考吗???

  • 后面新的DSP不再提供CSL库,而是提供基于register level的函数。 

    TI有提供edma driver。
    http://processors.wiki.ti.com/index.php/TI81XX_PSP_EDMA_Driver_User_Guide

    DM8168属于davinci系列,建议到davinci论坛提问。 

  • 请问怎么解决的?