This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X系统时间跳变

Other Parts Discussed in Thread: AM3354

板子上的芯片是AM3354,使用外部RTC,rx8010,但是最近发现一个问题,系统时间跳变。例如上电后设置时间为2016-11-5,和RTC 通过hwclock -w同步, 系统不断电运行2天,RTC时间是2016-11-7,通过hwclock -r 查询,但是通过date命令查询,系统时间跳变为2016-11-9。请问大家有没有遇到过这样的情况,谢谢!

  • 首先确认下你硬件上24M主时钟的晶体地和数字地共地了么?

    看下errata的描述:

    Advisory 1.0.30

    OSC0 and OSC1: Noise Immunity Improved When Crystal Circuit is Connected
    Directly to PCB Digital Ground

  • 您好,我也遇到同样的问题,AM335X Linux在启动时,使用了hwlock -s命令,使系统时间和RTC时间一致,但是经过一段时间后,发现系统时间和RTC的时间不一致,需要时间比RTC时间快,第一次快大概32个小时, 后面又会恢复保持一致,但隔一段时间后,系统时间又快大约30多个小时....。请问这是什么原因.