地址偏移量从0x24 直接跳到 0x2c,和技术手册上的不一样。
是因为库的版本问题吗??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
哦....
这里应该是hw_upp.h定义错了,starterware里没有upp的driver和example,估计也就没有测试发现这个错误。
BSL里的evmc6748_uPP.h定义就是对的,因为EVM板的BSL是有测试过的。
typedef struct
{
volatile uint32_t UPPID; // 0x0000
volatile uint32_t UPPCR; // 0x0004
volatile uint32_t UPDLB; // 0x0008
volatile uint32_t NA1; // 0x000c not accessable
volatile uint32_t UPCTL; // 0x0010
volatile uint32_t UPICR; // 0x0014
volatile uint32_t UPIVR; // 0x0018
volatile uint32_t UPTCR; // 0x001c
volatile uint32_t UPISR; // 0x0020
volatile uint32_t UPIER; // 0x0024
volatile uint32_t UPIES; // 0x0028
volatile uint32_t UPIEC; // 0x002c
volatile uint32_t UPEOI; // 0x0030
volatile uint32_t NA2; // 0x0034 not accessable
volatile uint32_t NA3; // 0x0038 not accessable
volatile uint32_t NA4; // 0x003c not accessable
volatile uint32_t UPID0; // 0x0040
volatile uint32_t UPID1; // 0x0044
volatile uint32_t UPID2; // 0x0048
volatile uint32_t NA5; // 0x004c not accessable
volatile uint32_t UPIS0; // 0x0050
volatile uint32_t UPIS1; // 0x0054
volatile uint32_t UPIS2; // 0x0058
volatile uint32_t NA6; // 0x005c not accessable
volatile uint32_t UPQD0; // 0x0060
volatile uint32_t UPQD1; // 0x0064
volatile uint32_t UPQD2; // 0x0068
volatile uint32_t NA7; // 0x007c not accessable
volatile uint32_t UPQS0; // 0x0070
volatile uint32_t UPQS1; // 0x0074
volatile uint32_t UPQS2; // 0x0078
} uPP_regs_t;
自已手动改一下吧。