This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pruss内核启动时加载失败

Other Parts Discussed in Thread: AM3354, AM3356

使用的am3354芯片,在TI的demo板没什么问题,这是怎么回事?

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.19-rt25-gf572d285f0 (pc335@pc335-hust) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #3 PREEMPT RT Mon Nov 14 11:14:50 CST 2016
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 24 MiB at 0x9e800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] On node 0 totalpages: 131072
[ 0.000000] free_area_init_node: node 0, pgdat c0929114, node_mem_map de36d000
[ 0.000000] Normal zone: 1152 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 131072 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=47596c59-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 484756K/524288K available (6419K kernel code, 323K rwdata, 2348K rodata, 260K init, 311K bss, 14956K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0898004 (8769 kB)
.init : 0xc0899000 - 0xc08da000 ( 260 kB)
.data : 0xc08da000 - 0xc092acc0 ( 324 kB)
.bss : 0xc092acc0 - 0xc0978b54 ( 312 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU kthread priority: 1.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000033] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000040] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000209] clocksource_probe: no matching clocksources found
[ 0.000424] Console: colour dummy device 80x30
[ 0.000608] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000610] This ensures that you still see kernel messages. Please
[ 0.000612] update your kernel commandline.
[ 0.119088] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.119094] pid_max: default: 32768 minimum: 301
[ 0.119244] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119251] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.120098] Initializing cgroup subsys io
[ 0.120123] Initializing cgroup subsys memory
[ 0.120164] Initializing cgroup subsys devices
[ 0.120178] Initializing cgroup subsys freezer
[ 0.120191] Initializing cgroup subsys perf_event
[ 0.120200] Initializing cgroup subsys pids
[ 0.120283] CPU: Testing write buffer coherency: ok
[ 0.120712] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.123812] devtmpfs: initialized
[ 0.137268] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.152758] omap_hwmod: debugss: _wait_target_disable failed
[ 0.209303] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.211958] pinctrl core: initialized pinctrl subsystem
[ 0.213551] NET: Registered protocol family 16
[ 0.216250] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.222415] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.223052] OMAP GPIO hardware version 0.1
[ 0.223905] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.225033] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.226270] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.233131] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe
[ 0.235721] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.279551] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.280005] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@0[0]'
[ 0.280387] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@1[0]'
[ 0.280681] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@2[0]'
[ 0.280950] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@3[0]'
[ 0.284178] usbcore: registered new interface driver usbfs
[ 0.284275] usbcore: registered new interface driver hub
[ 0.284475] usbcore: registered new device driver usb
[ 0.284954] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.285109] media: Linux media interface: v0.10
[ 0.285187] Linux video capture interface: v2.00
[ 0.285248] pps_core: LinuxPPS API ver. 1 registered
[ 0.285257] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.285290] PTP clock support registered
[ 0.285354] EDAC MC: Ver: 3.0.0
[ 0.286741] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.287129] Advanced Linux Sound Architecture Driver Initialized.
[ 0.288565] clocksource: Switched to clocksource timer1
[ 0.301872] NET: Registered protocol family 2
[ 0.302891] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.302975] TCP bind hash table entries: 4096 (order: 4, 98304 bytes)
[ 0.303190] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.303285] UDP hash table entries: 256 (order: 2, 16384 bytes)
[ 0.303330] UDP-Lite hash table entries: 256 (order: 2, 16384 bytes)
[ 0.303585] NET: Registered protocol family 1
[ 0.304174] RPC: Registered named UNIX socket transport module.
[ 0.304192] RPC: Registered udp transport module.
[ 0.304200] RPC: Registered tcp transport module.
[ 0.304207] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.304237] PCI: CLS 0 bytes, default 64
[ 0.305330] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.307768] futex hash table entries: 256 (order: 1, 8192 bytes)
[ 0.317704] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.318857] NFS: Registering the id_resolver key type
[ 0.318965] Key type id_resolver registered
[ 0.318975] Key type id_legacy registered
[ 0.319080] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.323596] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.323631] io scheduler noop registered
[ 0.323645] io scheduler deadline registered
[ 0.323956] io scheduler cfq registered (default)
[ 0.325548] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.402157] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.406241] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.019574] console [ttyS0] enabled
[ 1.024278] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.034247] [drm] Initialized drm 1.1.0 20060810
[ 1.040150] panel panel: GPIO lookup for consumer enable
[ 1.040170] panel panel: using device tree for GPIO lookup
[ 1.040185] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/panel[0]'
[ 1.040197] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/panel[0]'
[ 1.040208] panel panel: using lookup tables for GPIO lookup
[ 1.040221] panel panel: lookup for GPIO enable failed
[ 1.041879] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.048546] [drm] No driver support for vblank timestamp query.
[ 1.064931] Console: switching to colour frame buffer device 100x37
[ 1.075423] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.108607] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.122981] loop: module loaded
[ 1.129789] libphy: Fixed MDIO Bus: probed
[ 1.198602] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.204750] davinci_mdio 4a101000.mdio: detected phy mask fffffffd
[ 1.211933] libphy: 4a101000.mdio: probed
[ 1.215985] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver TI TLK10X 10/100 Mbps PHY
[ 1.226541] cpsw 4a100000.ethernet: No slave[1] phy_id, phy-handle, or fixed-link property
[ 1.234883] cpsw 4a100000.ethernet: Detected MACID = a0:f6:fd:4b:88:be
[ 1.243822] mousedev: PS/2 mouse device common for all mice
[ 1.250392] usbcore: registered new interface driver usbtouchscreen
[ 1.256752] i2c /dev entries driver
[ 1.261690] pinctrl-single 44e10800.pinmux: bad data for mux pinmux_mmc1_pins
[ 1.268880] pinctrl-single 44e10800.pinmux: no pins entries for pinmux_mmc1_pins
[ 1.276493] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.276509] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.276546] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
[ 1.276640] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.281289] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[ 1.281304] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.281316] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
[ 1.281328] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
[ 1.281339] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[ 1.281352] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
[ 1.326457] NET: Registered protocol family 10
[ 1.335744] sit: IPv6 over IPv4 tunneling driver
[ 1.341424] NET: Registered protocol family 17
[ 1.346283] Key type dns_resolver registered
[ 1.350917] omap_voltage_late_init: Voltage driver support not added
[ 1.355990] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.357909] mmc0: new high speed SDHC card at address 0002
[ 1.368889] mmcblk0: mmc0:0002 N/A 7.44 GiB
[ 1.374252] mmcblk0: p1 p2
[ 1.384297] pinctrl-single 44e10800.pinmux: pin 44e10874.0 already requested by 44e10800.pinmux; cannot claim for 50000000.gpmc
[ 1.395973] pinctrl-single 44e10800.pinmux: pin-29 (50000000.gpmc) status -22
[ 1.403157] pinctrl-single 44e10800.pinmux: could not request pin 29 (44e10874.0) from group nandflash_pins_s0 on device pinctrl-single
[ 1.415477] omap-gpmc 50000000.gpmc: Error applying setting, reverse things back
[ 1.423096] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.428270] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.434400] gpiochip_find_base: found new base at 510
[ 1.434609] gpiochip_add: registered GPIOs 510 to 511 on device: omap-gpmc
[ 1.435931] omap2-nand 8000000.nand: GPIO lookup for consumer rb
[ 1.435956] omap2-nand 8000000.nand: using device tree for GPIO lookup
[ 1.435997] of_get_named_gpiod_flags: parsed 'rb-gpios' property of node '/ocp/gpmc@50000000/nand@0,0[0]' - status (0)
[ 1.436065] nand: No NAND device found
[ 1.439846] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.448261] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.454782] hctosys: unable to open rtc device (rtc0)
[ 1.465217] vbat: disabling
[ 1.468065] vadc_fixed: disabling
[ 1.471548] vcpu_fixed: disabling
[ 1.475093] ALSA device list:
[ 1.478078] No soundcards found.
[ 12.317999] EXT4-fs (mmcblk0p2): recovery complete
[ 12.844570] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 12.852807] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 12.876967] devtmpfs: mounted
[ 12.880384] Freeing unused kernel memory: 260K (c0899000 - c08da000)
[ 13.227107] systemd[1]: System time before build time, advancing clock.
[ 13.332566] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 13.352392] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 13.375261] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLK)
[ 13.394283] systemd[1]: Detected architecture arm.
[ 13.420390] systemd[1]: Set hostname to <am335x-evm>.
[ 13.559495] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 33 bits of entropy available)
[ 13.567635] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 33 bits of entropy available)
[ 13.590215] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 33 bits of entropy available)
[ 13.610589] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 34 bits of entropy available)
[ 13.632980] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 34 bits of entropy available)
[ 13.807465] random: systemd: uninitialized urandom read (16 bytes read, 39 bits of entropy available)
[ 13.817669] random: systemd: uninitialized urandom read (16 bytes read, 39 bits of entropy available)
[ 13.828879] random: systemd: uninitialized urandom read (16 bytes read, 39 bits of entropy available)
[ 14.117589] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[ 14.457714] systemd[1]: rpcbind.socket: Found ordering cycle on rpcbind.socket/start
[ 14.465699] systemd[1]: rpcbind.socket: Found dependency on sysinit.target/start
[ 14.473197] systemd[1]: rpcbind.socket: Found dependency on alignment.service/start
[ 14.480930] systemd[1]: rpcbind.socket: Found dependency on basic.target/start
[ 14.488201] systemd[1]: rpcbind.socket: Found dependency on sockets.target/start
[ 14.495650] systemd[1]: rpcbind.socket: Found dependency on rpcbind.socket/start
[ 14.503102] systemd[1]: rpcbind.socket: Breaking ordering cycle by deleting job alignment.service/start
[ 14.512565] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with rpcbind.socket/start
[ 14.555834] systemd[1]: Listening on udev Kernel Socket.
[ 14.582582] systemd[1]: Created slice System Slice.
[ 14.609828] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 14.640840] systemd[1]: Created slice User and Session Slice.
[ 14.669232] systemd[1]: Reached target Slices.
[ 14.699730] systemd[1]: Listening on Journal Socket.
[ 14.754667] systemd[1]: Starting Load Kernel Modules...
[ 14.795367] systemd[1]: Starting Create list of required static device nodes for the current kernel...
[ 14.849581] cryptodev: driver 1.8 loaded.
[ 14.914504] systemd[1]: Mounting Temporary Directory...
[ 14.949883] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 14.989703] systemd[1]: Listening on Syslog Socket.
[ 15.021325] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 15.049789] systemd[1]: Listening on udev Control Socket.
[ 15.084707] systemd[1]: Mounting POSIX Message Queue File System...
[ 15.131352] systemd[1]: Created slice system-getty.slice.
[ 15.159309] systemd[1]: Reached target Swap.
[ 15.179227] systemd[1]: Reached target Remote File Systems.
[ 15.223747] systemd[1]: Starting Setup Virtual Console...
[ 15.270019] systemd[1]: Listening on Journal Socket (/dev/log).
[ 15.304995] systemd[1]: Starting Journal Service...
[ 15.340071] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 15.399509] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 15.460211] systemd[1]: Listening on Network Service Netlink Socket.
[ 15.477904] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 15.539557] systemd[1]: Reached target Paths.
[ 15.574873] systemd[1]: Mounting Debug File System...
[ 15.691645] systemd[1]: Mounted Debug File System.
[ 15.719512] systemd[1]: Mounted POSIX Message Queue File System.
[ 15.749459] systemd[1]: Mounted Temporary Directory.
[ 15.780208] systemd[1]: Started Journal Service.
[ 17.641079] systemd-journald[126]: Received request to flush runtime journal from PID 1
[ 20.908953] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 20.993421] rtc rtc0: 44e3e000.rtc: dev (254:0)
[ 20.993484] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 21.019089] input: ti-tsc as /devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input0
[ 21.218085] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset
[ 21.218125] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 21.218144] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 21.218158] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 21.218169] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 21.218183] am335x-phy-driver 47401300.usb-phy: lookup for GPIO reset failed
[ 21.218196] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect
[ 21.218207] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 21.218218] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 21.218229] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 21.218240] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 21.218252] am335x-phy-driver 47401300.usb-phy: lookup for GPIO vbus-detect failed
[ 21.218332] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 21.313934] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset
[ 21.313975] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 21.313994] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 21.314008] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 21.314019] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 21.314033] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO reset failed
[ 21.314048] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect
[ 21.314058] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 21.314069] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 21.314081] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 21.314092] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 21.314103] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO vbus-detect failed
[ 21.314181] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 21.541357] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 22.096065] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 22.375359] remoteproc0: wkup_m3 is available
[ 22.432444] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 22.432453] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 22.657946] remoteproc0: powering up wkup_m3
[ 22.666427] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217152
[ 22.666737] remoteproc0: remote processor wkup_m3 is now up
[ 22.666809] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x191
[ 23.142259] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 23.541184] omap_hwmod: pruss: _wait_target_ready failed: -16
[ 23.573334] ti-pruss 4a300000.pruss: couldn't enable pruss
[ 23.642666] ti-pruss: probe of 4a300000.Pruss failed with error -16
[ 23.739658] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 23.815676] PM: bootloader does not support rtc-only!
[ 25.055703] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 28.059539] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 28.059578] musb-hdrc: MHDRC RTL version 2.0
[ 28.059590] musb-hdrc: setup fifo_mode 4
[ 28.059614] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 28.068378] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver
[ 28.076759] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1
[ 28.161743] hub 1-0:1.0: USB hub found
[ 28.198794] hub 1-0:1.0: 1 port detected
[ 28.303546] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 28.303584] musb-hdrc: MHDRC RTL version 2.0
[ 28.303597] musb-hdrc: setup fifo_mode 4
[ 28.303622] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 28.315817] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 28.346107] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 28.415802] hub 2-0:1.0: USB hub found
[ 28.445426] hub 2-0:1.0: 1 port detected
[ 28.868988] usb 2-1: new high-speed USB device number 2 using musb-hdrc
[ 29.032817] hub 2-1:1.0: USB hub found
[ 29.046407] hub 2-1:1.0: 4 ports detected
[ 29.339041] usb 2-1.1: new low-speed USB device number 3 using musb-hdrc
[ 29.460179] input: eGalax Inc. USB TouchController as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1.auto/usb2/2-1/2-1.1/2-1.1:1.0/input/input1
[ 29.588857] usb 2-1.4: new low-speed USB device number 4 using musb-hdrc
[ 29.937872] input: PixArt USB Optical Mouse as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1.auto/usb2/2-1/2-1.4/2-1.4:1.0/0003:093A:2510.0001/input/input2
[ 29.957902] hid-generic 0003:093A:2510.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-musb-hdrc.1.auto-1.4/input0
[ 29.979643] usbcore: registered new interface driver usbhid
[ 29.985277] usbhid: USB HID core driver
[ 31.227650] NET: Registered protocol family 15
[ 31.270992] random: nonblocking pool is initialized
[ 32.083071] net eth0: initializing cpsw version 1.12 (0)
[ 32.088449] net eth0: initialized cpsw ale version 1.4
[ 32.106056] net eth0: ALE Table size 1024
[ 32.229237] net eth0: phy found : id is : 0x2000a211
[ 32.234348] libphy: PHY not found
[ 32.237774] net eth0: phy "" not found on slave 1, err -19
[ 32.303383] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 32.721417] Bluetooth: Core ver 2.21
[ 32.774602] NET: Registered protocol family 31
[ 32.821366] Bluetooth: HCI device and connection manager initialized
[ 32.884233] Bluetooth: HCI socket layer initialized
[ 32.916798] Initializing XFRM netlink socket
[ 32.931156] using random self ethernet address
[ 32.931167] using random host ethernet address
[ 32.931211] using host ethernet address: A0:F6:FD:4B:88:C0
[ 32.931212] using random self ethernet address
[ 32.931219] using random host ethernet address
[ 32.957497] using host ethernet address: A0:F6:FD:4B:88:C0
[ 32.957499] usb0: HOST MAC a0:f6:fd:4b:88:c0
[ 32.957589] usb0: MAC d2:11:5a:74:f3:f4
[ 33.094954] Mass Storage Function, version: 2009/09/11
[ 33.094968] LUN: removable file: (no medium)
[ 33.095273] LUN: removable read only file: /dev/mmcblk0p1
[ 33.095280] Number of LUNs=1
[ 33.108399] g_multi gadget: Multifunction Composite Gadget
[ 33.108410] g_multi gadget: g_multi ready
[ 33.536524] Bluetooth: L2CAP socket layer initialized
[ 33.574702] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
[ 33.645802] Bluetooth: SCO socket layer initialized
[ 34.229625] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 34.261718] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 40.572947] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]