This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
环境:dm8168 + dvrrdk4.0.2
我现在想在嵌入式linux开发板根目录下新建一个/Userdata目录,然后把/dev/mtdblock7挂载到/Userdata
在/Userdata保存应用程序的配置数据,可是有时候断电再送电 保存在 /Userdata目录的文件打不开
出现input/output error,请问是为什么?
如果这种方法不行,想要在一个分区中保存数据,还有没有其他方法?
下面是我系统启动的时候运行的脚本
mkdir /Userdata
chmod -R 777 /Userdata
mount -t ext2 /dev/mtdblock7 /Userdata -o sync
if [ $? -eq 0 ]
then
echo "this is N time to use"
else
echo "this is first to use"
mkfs.ext2 /dev/mtdblock7
mount -t ext2 /dev/mtdblock7 /Userdata -o sync
fi
你好! 我已经加了同步信号sync ,并且还延时3S左右才去断电,不可能没有写进去
我再/Userdata 目录下vi 123.txt 保存延时3S,再断电上电也会出现input/output error,