Hi,
I'm working on custom DM385 board which uses 8-bit nand. Two boards with different NAND chip.(S34ML01G1 & MT29F1G08) but not a single NAND is getting detected. if we use same uboot in x16 bit DM385 board. It is detecting NAND.
When we read maf_id and device_id i get 0x17 & 0x17 in uboot.
GPMC_CONFIG1 -> 0x00000800
CONTROL_STATUS -> 0x00000317
UBOOT -> arago-project.org/.../
KERNEL -> arago-project.org/.../
can anybody help to solve these.
Thanks & regards,
Ganesh