This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385的IPNC RDK环境如何实现UVC的MJPEG解码显示及H264编码存储和传输??



大家好,我现在需要用DM385的环境搭建一个USB的摄像头输入,带3寸的屏显示。USB摄像头输出是MJPEG 720P30的格式,现在的问题是,怎么用RDK的环境和接口实现MJPEG的解码显示,另外需要转成H.264的编码存储和传输。看了IPNC_RDK_GA_Release3.8.0里面的所有文档及代码都没有找到相关的说明和应用代码,目前看到的似乎只支持CVBS输入和CMOS的方式,那么UVC的方式,该如果操作呢?请各位有经验的前辈多多指点啊!TI的环境还不熟,请大家多多指教!谢谢!

  • Chen Kingco,

    DM385的linux 基于标准的linux kernel,其中的UVC支持也是标准linux支持的功能,你可以到网上搜索一下相关信息。

    关于解码,IPNC软件里面有解码的link,但是没有相关的demo。如果你有DVR RDK的软件的话,里面有解码的demo。