问下,1、6655的 EDMA 能不能把数据从 DDR 搬移到 L1 SRAM中,还是只能搬到L2 SRAM中。
2、6655的Cache使用有没有相关例程的,包括CSL库或其他函数配置。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问下,1、6655的 EDMA 能不能把数据从 DDR 搬移到 L1 SRAM中,还是只能搬到L2 SRAM中。
2、6655的Cache使用有没有相关例程的,包括CSL库或其他函数配置。
1. 可以,但是需要将L1设置为SRAM而不是Cache,实际上这么做降低太多的性能,所以很少会这样设置;
2. 参考首页K1 STK开发包,C6657的可以用在C6655上。