您好,我在6678上跑的hua结果运行对吗?
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PA successfully initialized
[C66xx_0] HUA version 2.00.00.03
[C66xx_0] Setting hostname to tidemo-
[C66xx_0] MAC Address: 90-D7-EB-2C-68-A8
[C66xx_0] EVM in StaticIP mode at 192.168.2.100
[C66xx_0] Set IP address of PC to 192.168.2.101
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
[C66xx_0] Network Added: If-1:192.168.2.100
[C66xx_0] Service Status: THTTP : Enabled : : 000
为什么不能ping通 也不能link网页?会不会是phy硬件接口有问题呢